Toshiba Announces 10TB Enterprise Capacity HDD Generation With SATA Model Line-up

New MG06 Series delivers 25 percent capacity increase over prior generation models

Monday, September 25, 2017 10:00 pm EDT

Dateline:

IRVINE, Calif.
"Committed to People, Committed to the Future"

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today announces the 10TB 1 MG06 Series Enterprise Capacity HDD model line-up. Toshiba’s new MG06 series offers a 25 percent capacity increase compared to prior generations and enables models to be delivered at multiple capacity points to better leverage capacity refresh qualification cycles for OEMs/ODMs infrastructure builders, cloud solution providers (CSPs) and system integrators.

In addition to a heftier capacity, the 10TB MG06 Series features a greater maximum sustained transfer rate, 237 MiB/s2, than the earlier MG05 Series, as well as a 25 percent increase in MTTF3, with a rating of 2.5M hours. The drive provides a SATA 6Gbit/s interface4 and 7,200 rpm performance. Additionally, the MG06 HDD supports emulated 512 Advanced Format (512e) technology for compatibility with legacy applications and operating environments; or 4K native sector technology for optimum performance in all-disk or hybrid storage platforms.

“The volume and value of digital data across organizations of all sizes continues to create opportunities and challenges for CSPs, server and storage vendors, and IT professionals,” said Scott Wright, Director of HDD Product Marketing at Toshiba America Electronic Components, Inc. “Toshiba’s new MG06 Series advances performance and value across a range of Enterprise Capacity HDD models to better align with the diverse needs of systems and solutions for Cloud and Business Critical applications today.”

Designed to support higher storage density, the MG06 Series HDD introduces 10TB to Toshiba’s line-up while also updating 6TB and 8TB capacities. Based on Toshiba’s latest HDD architecture, the new models can save rack space to improve the operational efficiency of cloud-scale infrastructure. The MG06 Series is engineered for mid-line, nearline, and tier two business critical server and storage system workloads; including servers supporting application workloads that benefit from high capacity per spindle; capacity-optimized data center storage systems; and enterprise IT and data center servers supporting workloads per HDD of up to 550TB total bytes written and read per year. All models feature Toshiba’s Persistent Write Cache Technology for peak performance and enterprise-grade data reliability. Models also support power mode management capabilities that conform to HDD industry standards.

Sample shipments of the MG06 SATA HDD model are now available. For more information on Toshiba’s line of storage product, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba’s storage solutions visit the storage blog at http://storage.toshiba.com/corporateblog/ and follow @ToshibaStorage on Twitter.

About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives. Visit Toshiba's web site at http://toshiba.semicon-storage.com.

© 2017 Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

1 Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 230 bytes = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.

2 A kibibyte (KiB) means 210, or 1,024 bytes, a mebibyte (MiB) means 220, or 1,048,576 bytes, and a gibibyte (GiB) means 230, or 1,073,741,824 bytes.

3 MTTF (Mean Time to Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may be different from the MTTF.

4 Read and write speed may vary depending on the host device, read and write conditions, and file size.

Multimedia Files:

Preview image
SATA Interface
Preview image

Contact:

WE Communications
Sarah Elson, 415-638-7407
selson@we-worldwide.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter