Toshiba Announces First MN Series HDDs Expanding Disk Drive Model Category Line-up

The MN HDD Series, available in 4TB 1 , 6TB and 8TB, defines a new value point in Toshiba’s capacity Client HDD model categories

Tuesday, February 7, 2017 9:00 pm EST


IRVINE, Calif.
"Many customers with predominantly file-oriented and fixed-content sequential write and read workloads are looking for cost-effective capacity for moderate workload storage applications"

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today announces its first MN Series HDDs, bridging the value gap between top-end enterprise capacity HDDs and entry-level desktop HDDs, while still delivering 7,200RPM rotational latency performance.

The MN series delivers up to 8TB capacity in a 3.5-inch form factor for a broad range of file and object storage applications. With a 6 Gbit/s2 SATA interface, 7,200 rotational speed, 1,000,000 hour MTTF3 rating, and a rated annual workload of 180TB4 transferred, the new HDD series delivers the performance and reliability needed for file and object storage workloads that typically utilize sequential data transfer operations. The drives are designed for 24/7 power-on operation and feature rotational vibration compensation technology to help provide consistent performance in tower and low-density style multi-drive enclosures, such as small NAS platforms.

“Many customers with predominantly file-oriented and fixed-content sequential write and read workloads are looking for cost-effective capacity for moderate workload storage applications,” said Scott Wright, director of HDD marketing at Toshiba America Electronic Components, Inc. With our new MN Series HDD models we are providing a workload range within the high workload data center work-horse Enterprise Capacity HDDs and relatively low workloads associated with client HDD models.”

The initial MN Series HDD models are available in 8TB, 6TB and 4TB capacities, each leveraging Toshiba’s proven Enterprise Capacity category HDD design legacy to deliver highly cost-effective storage for fixed-content workload-limited use cases. Targeted applications include mid-level, entry-level and SOHO NAS storage enclosures, remote-office back-up and archival storage, and home multimedia data archive and fixed-content object storage.

For more information on Toshiba’s line of industry-leading HDDs, please visit: To learn more about Toshiba’s storage solutions follow @ToshibaStorage on Twitter.

About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide. Visit Toshiba's web site at

© 2017 Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

1 Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.

2 Read and write speed may vary depending on the host device, read and write conditions, and file size.

3 MTTF (Mean Time to Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may be different from the MTTF.

4 Workload is a measure of the data throughput of the year, and it is defined as the amount of data written, read or verified by commands from host system.


WE Communications
Amanda Gonzalez, 415-547-7020

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter