Toshiba is the Fastest Growing HDD and SSD Vendor of 2016

New Reports Identify Toshiba as the Growth Leader 1 in Hard Disk and Solid State Drive Market Segments

Tuesday, March 7, 2017 9:00 am EST


IRVINE, Calif.
"The rapid growth we achieved across both our HDD and SSD portfolios is a result of the trust our customers have in the Americas and worldwide Toshiba teams to provide a broad array of products that help them scale quickly and remain competitive in a fast-paced environment"

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba America Electronic Components, Inc. (TAEC) today announces that Toshiba, a committed technology leader, was the fastest growing vendor in both the worldwide $25 billion hard disk drive (HDD) segment, as well as in the $17 billion solid state drive (SSD) segment in 2016 over 2015, as measured by revenue and units. These accolades were recognized in two recent IDC reports: “Worldwide Solid State Storage Quarterly Update, CY 4Q16 2” and “Worldwide 4Q16 HDD Shipment Results and Four-Quarter Forecast Update 3.”

"Toshiba's broad HDD and SSD portfolio enabled them to participate in nearly all market segments for storage devices, a key factor that helped to underpin Toshiba's strong year-over-year revenue growth in CY2016," according to John Rydning and Jeff Janukowicz, research vice presidents at IDC. "With successful launches of new HDD and SSD products over the next few quarters to address demand from cloud service providers and the traditional IT market, Toshiba should be well positioned to sustain further HDD and SSD revenue growth in 2017."

In the HDD segment, Toshiba’s unit market share increased by 9 percentage points in the fourth quarter 2016, reaching a total market share of 24 percent, a 60 percent increase from the second quarter 2015 share of 15 percent. Toshiba was the only HDD vendor to grow in total revenue in 2016 and increase revenue share in every product segment including mobile, desktop, performance-optimized enterprise and capacity-optimized enterprise for the year. The SSD business also realized strong growth. Toshiba grew SSD revenue 114% year over year in 2016, reaching the fourth share position in the market.

“The rapid growth we achieved across both our HDD and SSD portfolios is a result of the trust our customers have in the Americas and worldwide Toshiba teams to provide a broad array of products that help them scale quickly and remain competitive in a fast-paced environment,” said Steve Fingerhut, senior vice president and general manager, HDD and SSD business units at Toshiba America Electronic Components, Inc. “These results are just the beginning as we will continue to roll out innovative storage products that enable the rapid data growth required by Client, Cloud Data Center and Enterprise applications.”

As a global technology company that has been innovating in storage for years, Toshiba offers a comprehensive portfolio of HDD and SSD products that address the storage needs of enterprise, Data Center, and client markets. The company solves customer challenges with innovative HDD models focusing on four primary market segments: The AL Series focuses on the Enterprise Performance segment; the MG Series is aimed at Enterprise Capacity and Data Center needs; the MQ Series covers the broad spectrum of use cases that require Mobile Client HDDs; and the DT Series addresses the traditional Desktop Client use case. Toshiba’s SSD solutions also span multiple market segments and include the PX Series of SAS SSDs, which provide excellent performance and capacity for enterprise and hyper-converged environments; the ZD6300 Series, which is the highest4 capacity, native dual port Non-Volatile Memory Express® (NVMe5) SSD at 7.68TB6 in a 2.5 inch form factor; and the BG series, which is the smallest7 multi-lane Peripheral Component Interconnect Express® (PCIe®8) NVMe SSD in production designed for client drive and server boot drive applications.

For more information on Toshiba’s line of storage product, please visit: To learn more about Toshiba’s storage solutions visit the storage blog at and follow @ToshibaStorage on Twitter.

About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide. Visit Toshiba's web site at

© 2017 Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

1 2015 revenue and unit baseline includes separate results from companies merged in 2016

2 Worldwide Solid State Storage Quarterly Update, CY 4Q16 (Feb 2017 - Doc # US41259317)

3 Worldwide 4Q16 HDD Shipment Results and Four-Quarter Forecast Update (Feb 2017 - Doc # US42306617)

4 As of Toshiba Survey, February 14, 2017

5 NVMe and NVM Express are a trademark of NVM Express, Inc.

6 Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240 = 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.

7 As of Toshiba Survey, February 14, 2017

8 PCIe and PCI Express are a registered trademark of PCI-SIG


WE Communications
Amanda Gonzalez, 415-547-7020

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter