Toshiba Introduces the OCZ VX500 SATA SSD Series

New Toshiba-OCZ SSD Solution Features Excellent Balance of Performance and Endurance for Mainstream Systems

Tuesday, September 13, 2016 9:00 am EDT

Dateline:

SAN JOSE, Calif.
"Delivering over 3X the endurance of TLC-based SSDs7, the Toshiba OCZ VX500 SSD series ensures users who need increased product longevity aren’t neglected in the wake of a value-oriented market"

SAN JOSE, Calif.--(BUSINESS WIRE)--Toshiba America Electronic Components, Inc. (TAEC), a committed technology leader, today announces the launch of the OCZ VX500 SATA solid state drive (SSD) series. Aimed at mainstream desktop and notebook users looking to migrate away from primary hard disc drive (HDD) usage, VX500 SSDs feature superior endurance ratings1 and provide a faster, more responsive PC experience thanks to well-balanced read and write performance2.

Backed by OEM-level testing that provides validated reliability and built with the latest Toshiba MLC NAND flash, the Toshiba OCZ VX500 SSD series delivers endurance ratings of 74 to 592 terabytes written (TBW)3, making it suitable for write-intensive applications such as content creation, revolving media/game storage, or as a scratch disk.

The Toshiba OCZ VX500 series is designed to thrive in mixed workload environments representative of mainstream users who need increased performance4 to take their everyday computing to the next level. With sequential read/write speeds of up to 550 MB/s and 515 MB/s, and random read/write performance of up to 92,000 and 65,000 4KiB5 input/output operations per second (IOPS)6, VX500 SSDs can significantly boost system productivity compared to HDD storage. Users can also count on enhanced durability and power consumption over their hard drives, as well as quality lightweight housing weighing in at only 54g.

“Delivering over 3X the endurance of TLC-based SSDs7, the Toshiba OCZ VX500 SSD series ensures users who need increased product longevity aren’t neglected in the wake of a value-oriented market,” said Alex Mei, VP of Marketing and GM of Etail/Retail SSDs at Toshiba America Electronic Components, Inc. “The VX500 series was designed for today’s DIYers looking to upgrade from traditional hard drives with a solid state solution that thrives in the wide spectrum of mainstream oriented mixed workload applications.”

The OCZ VX500 SATA SSD series will be available in four different capacities ranging from 128GB to 1024GB8 and will be backed by a 5-year Advanced Warranty Program9, created to provide reliable customer service and mitigates the frustration surrounding warranty and support claims. Additionally, each VX500 SSD comes bundled with Acronis® True Image™10 cloning software for users to easily transfer their data to the new SSD and enjoy a smooth upgrade experience.

About Toshiba Corp. and Toshiba America Electronic Components, Inc. (TAEC)

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 580 consolidated companies employing over 199,000 people worldwide. Visit Toshiba's web site at http://toshiba.semicon-storage.com.

About OCZ

OCZ is an enthusiast SSD brand offered by Toshiba for the consumer market. More information is available at www.ocz.com.

© 2016 Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

1 Compared to current TLC-based SSDs

2 Read and write speed may vary depending on the host device, read and write conditions, and file size

3 Definition and conditions of TBW (Terabytes Written) are based on JEDEC standard; JESD218A, February 2011, and defined for the service life.

4 Compared to current TLC-based SSDs

5 A kibibyte (KiB) means 210, or 1,024 bytes, a mebibyte (MiB) means 220, or 1,048,576 bytes, and a gibibyte (GiB) means 230, or 1,073,471,824 bytes

6 Based on the 1024GB model, see ocz.com for full specifications

7 592 TBW vs. 150 TBW (leading TLC SSD based on 2016 sales volume)

8 Definition of capacity: Toshiba defines a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1,073,741,824 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.

9 Limited Warranty, full terms and conditions available at https://ocz.com/us/support/advanced-warranty

10 Acronis and True Image are registered trademarks or trademarks of Acronis International GmbH or its affiliates in the United States and other countries.

Contact:

TAEC - OCZ
Mia Cool, 408-733-8400 x351
mia.cool@taec.toshiba.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter

  • Looking for ways to prevent summer learning loss in your students? Here are nine resources ✏️you can pass along to… https://t.co/gtmi5PURoB5 hours 54 min ago
  • Who else started their day with eggs , toast and a hot cup of coffee ☕️? Our vintage toaster used to be the go-t… https://t.co/lVSr3Pr0MC8 hours 20 min ago
  • , what do you all think of this story? Could be a good part of your school’s lesson plans once back in sess… https://t.co/6T6hd4DYW213 hours 55 min ago
  • After-school activities are inspiring kids to keep learning. What engaging activities can you encourage your… https://t.co/aRgf5ZOGUb1 day 7 hours ago