Toshiba Announces Availability of dynaPad, World’s Thinnest and Lightest 12-Inch Tablet Powered by Windows

  • 12-inch Windows-powered tablet measures just 6.9mm (0.27 in) thin and weighs only 1.28 pounds
  • Delivers precision digital inking technologies by Wacom for a truly natural handwriting experience that feels like writing with pen on paper
  • Suite of Toshiba original business applications inspire creativity, productivity and collaboration
  • Available for pre-order starting today direct from Toshiba and at Microsoft Stores in late January for $569.99 MSRP

Tuesday, January 5, 2016 8:00 am EST

Dateline:

LAS VEGAS
"Advances in engineering and pen technology have enabled us to create an amazingly thin and light tablet that’s ideal for instant creativity while also offering the versatility to immediately transition to a clamshell form factor for productivity. Toshiba dynaPad is the ultimate digital notebook."

LAS VEGAS--(BUSINESS WIRE)--CONSUMER ELECTRONICS SHOW – Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the availability of dynaPad™, a light and powerful tablet powered by Windows 10 and engineered to deliver the natural feel of pen to paper so you can work and create freely.

“Precision digital inking technology is the next frontier of truly personal computing,” said Philip Osako, senior director of product marketing, Toshiba America Information Systems, Inc., Digital Products Division. “Advances in engineering and pen technology have enabled us to create an amazingly thin and light tablet that’s ideal for instant creativity while also offering the versatility to immediately transition to a clamshell form factor for productivity. Toshiba dynaPad is the ultimate digital notebook.”

Remarkably Accurate Pen Experience

Built with professional-grade digital inking technologies by Wacom®, Toshiba’s exclusive Active Electrostatics (ES) TruPen™ with Wacom® Feel delivers pen precision and accuracy, so note-taking, sketching and drawing feels like writing with pen on paper. Ideal for designers, artists and note-takers, it is also great for highlighting and writing notes directly on webpages through the annotating features in the Microsoft Edge browser. Featuring a sophisticated metal design, this fine-tip digitizer pen supports 2,048 levels of pressure sensitivity and writing or drawing capabilities from extreme angles with virtually no latency. And because the pen is battery-powered, it can last for more than 1,000 hours so there is no need to carry a separate charging connector.

“Our Active ES solution continues to deliver a best-in-class writing and drawing experience on tablets like the Toshiba dynaPad,” said Masahiko Yamada, president and CEO of Wacom Ltd. “Toshiba’s TruPen stylus delivers unprecedented accuracy and speed and allows users to create intricate details, just like they would with a pen or pencil on paper.”

Dynamic Full HD Display Precision Engineered for Handwriting

Toshiba dynaPad features a 12-inch Full HD+ (1920x1280) TruBrite® display1 remastered for handwriting. To achieve a digital canvas that best replicates the natural feel of pen to paper, Toshiba bonds two sheets of high-quality glass with a metal mesh sensor and incorporates Corning’s Gorilla Glass 3 with Native Damage Resistance™, plus an anti-fingerprint coating to deliver a sturdy surface that accepts fine lines and pressure-sensitive strokes – all while delivering a crystal clear 2 million pixel-perfect view.

The World’s Lightest 12-inch Windows Tablet

The innovative slim and lightweight design of dynaPad – 6.9mm thin and 1.28 pounds2 – makes dynaPad the world’s lightest 12-inch tablet that is powered by Windows3. Sized to mimic a traditional A4 paper size, dynaPad’s design complements the large display area with a carbon fiber housing and a sophisticated, rubberized finish to give it a solid feel in hand, while reducing flex.

The device also offers an optional ultra-thin, full-size keyboard with a 19mm pitch and 1.5mm stroke for easier typing and a well-sized touchpad ideal for Windows navigation. Attached by magnets, users can quickly convert the tablet to a clamshell laptop for productivity applications. The TruPen neatly attaches to the side of the tablet.

“Toshiba’s dynaPad is a great example of a device that highlights how Windows 10 can help people do great things,” said Peter Han, vice president of Worldwide OEM Marketing, Microsoft Corp. “Toshiba’s TruPen with Wacom Feel technology is fantastic for taking notes and highlighting on webpages in the Microsoft Edge browser and the detachable keyboard combined with Continuum on Windows 10 enables you to use it as a tablet or laptop.”

Toshiba’s Suite of Original Apps Designed for the Way You Work

The dynaPad also includes updated versions of Toshiba’s exclusive suite of original business applications that enable users to easily collect, organize and share notes, images and files and integrate them seamlessly with Microsoft Office. The suite includes:

  • TruNote™: A simple, yet powerful handwriting app lets you effortlessly take lecture or meeting notes, create detailed hand drawings, search handwritten messages4, manage multiple notebooks and more. Smart settings allow for left- or right-handed use to maintain a normal writing style.
  • TruCapture™: Easily capture images and text from whiteboards, textbooks, newspapers and more, at any angle for simple importing into presentations and sharing.
  • TruRecorder™: A powerful voice recording application for meetings, lectures and interviews that can recognize the speaker’s voice for easy playback.
  • TruNote Clip: Easily capture screen clips and mark them up for easy sharing.
  • TruNote Share: Turn the tablet into a real-time whiteboard that can be shared with up to 40 people.

Performance for Creativity and Productivity

The tablet features the Intel® Atom™ x5 Z8300 processor5 with up to 4GB of RAM6 and up to 64GB of flash storage7 delivering snappy performance for navigating Windows 10, using apps and getting work done. Offering a range of connectivity options, dynaPad includes two Micro USB 2.0 ports, a microSD card slot that supports up to 128GB cards and a Micro HDMI® port for connecting to external devices. In addition, the device includes ultrafast 802.11ac Wi-Fi® and Bluetooth as well as a 2MP front-facing camera and dual-array TruTalk™ mics for video chatting and an 8MP rear camera with auto-focus.

Pricing & Availability

Toshiba dynaPad is available today for pre-order starting today direct from Toshiba at toshiba.com/us and at Microsoft Stores in late January for $569.99 MSRP.

Image Gallery: http://bit.ly/ToshibadynaPad

Connect with Toshiba on Facebook at www.facebook.com/ToshibaUSA, on Twitter at twitter.com/ToshibaUSA, and on YouTube at youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of five business units: Business Solutions Division, Digital Products Division, Imaging Systems Division, Telecommunication Systems Division and Industrial Solutions & Services Division. Together, these divisions provide digital products, services and solutions, including award-winning notebook computers, tablets, branded storage products, digital display solutions and cloud services; imaging products for the security, medical and manufacturing markets; IP business telephone systems with unified communications, collaboration and mobility applications; and IoT solution development, data analytics and IT services. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation, a Fortune Global 500 company, channels world-class capabilities in advanced electronic and electrical product and systems into five strategic business domains: Energy & Infrastructure, Community Solutions, Healthcare Systems & Services, Electronic Devices & Components, and Lifestyles Products & Services. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future,” Toshiba promotes global operations and is contributing to the realization of a world where generations to come can live better lives. Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global network of over 580 consolidated companies employing 199,000 people worldwide, with annual sales surpassing 6.6 trillion yen (US$55 billion). To find out more about Toshiba, visit www.toshiba.co.jp/index.htm

© 2016 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

1 Display. Any small bright dots that may appear on your display are an intrinsic characteristic of the thin film transistors manufacturing technology. See Display Legal Footnote at www.info.toshiba.com
2 Weight. Weight may vary. See Weight Legal Footnote at www.info.toshiba.com
3 Based on Toshiba’s research as of November 18, 2015.
4 Handwriting search functionality is powered by MyScript®
5 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com
6 Memory. Memory size may vary. See Memory Legal Footnote at www.info.toshiba.com
7 Flash Memory Capacity. Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Solid State Drive Capacity Legal Footnote at www.info.toshiba.com

Contact:

Access Communications
Carina Uehara, 917-522-3538
cuehara@accesspr.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter

  • Woohoo! We always like to hear about teachers entering teams in https://t.co/AOCMtMVRfn! How many pr… https://t.co/KEfHea2Lrd30 min 45 sec ago
  • These students from skyped with a scientist all the way from Iceland in preparation for their upcomin… https://t.co/oPMWZjyFcv15 hours 52 min ago
  • We’ll ask around! Stay tuned for more.16 hours 7 min ago
  • , with the holidays are in full swing, what activities do you have planned to keep your Ss on task and engaged ❄️?16 hours 37 min ago