Press Release Search

all Press Releases

  • 12/13/10 9:00 pm EST
    IRVINE, Calif.--(BUSINESS WIRE)--Extending its position in the enterprise storage market, Toshiba Storage Device Division announces its new family of enterprise-class solid state drives (SSDs). Developed to meet the market’s demand for higher performance and lower power consumption, the new MKx001GRZB series combines Toshiba hard disk drive (HDD) expertise and its leadership as the inventor of NAND flash technology. The 2.5-inch small form factormore...
  • 11/30/10 9:10 am EST
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba Storage Device Division (SDD), the pioneer in small form factor hard disk drives (HDDs), today announced a 7,200 RPM 2.5-inch Self-Encrypting Drive (SED) that provides government-grade AES-256 hardware encryption incorporated in the disk drive’s controller electronics. Based on the Opal Security Subsystem Class (Opal SSC) specification from the Trusted Computing Group (TCG), the new Toshiba SED enables securemore...
  • 11/15/10 9:00 pm EST
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba Storage Device Division (SDD), the pioneer in small form factor hard disk drives (HDDs), today announced two new 2.5-inch HDD models designed for rugged 24-hour continuous operation in computing, industrial, and other extreme environments. The new models – the 100GB1 SATA interface MK1060GSCX and the 80GB1 PATA interface MK8050GACY – offer exceptional reliability and performance across wide temperature, altitudemore...
  • 10/12/10 3:04 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today introduced two 4G WiMAX-ready1 models of the Portégé® R700, the world’s lightest 13.3-inch full-performance ultraportable laptop with an integrated DVD drive2. The new Portégé R700 models not only provide business users with unprecedented performance and durability in a highly mobile form factor, but the most comprehensive connectivitymore...
  • 9/28/10 6:08 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba's Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today introduced Toshiba Book Place, an e-book reader and store that adds easy-to-access, interactive e-books to the suite of digital entertainment products that consumers can enjoy on laptops. In partnership with K-NFB Reading Technology, Inc., a joint venture between Kurzweil Technologies Inc. and the National Federation for the Blind, Toshibamore...
  • 9/28/10 2:45 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced that it has added powerful new features to enhance the 3D playback capabilities of its Satellite® A665-3D Series laptops. Equipped with NVIDIA® 3D Vision™ technology1, the updated laptop models are ready to deliver a stereoscopic 3D experience to games, movies, photos and more. New features further enhance the experience, givingmore...
  • 9/28/10 9:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--With the ever-increasing demands of digital media, Toshiba introduces the Canvio™ 3.0 portable hard disk drive (HDD) featuring a SuperSpeed USB 3.0 interface. For the same price as competing USB 2.0 drives, Canvio 3.0 drives offer blazing fast file transfers at up to 10 times the speed of USB 2.0 drives. Available in storage capacities of 500 gigabytes (GB1), 750GB or one terabyte (TB1), Canvio 3.0 drives feature simplemore...
  • 9/23/10 2:00 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the Satellite® L635 Kids’ PC, Toshiba’s first kid-centric laptop design, available exclusively at Best Buy. Designed in collaboration with Best Buy, the Satellite L635 Kids’ PC is a full-size laptop made for children aged five to 10 that provides a suite of entertainment and education software and allows parents to help ensuremore...
  • 9/22/10 8:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced its award-winning Qosmio® X500 Series laptops is getting a graphics performance boost from the new NVIDIA® GeForce™ GTX 460M graphics processor1 with 1.5GB of discrete graphics memory. The high-performance Qosmio X500 Series laptops deliver elite mobile performance and high-end features for demanding tasks – games, media creationmore...
  • 9/22/10 8:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today rolled out a range of premium 4G WiMAX™-ready laptops 1, designed to give consumers broader wireless coverage all over town, not just at wireless hotspots. “A WiMAX-equipped laptop gives on-the-go consumers the connection speeds they’re used to in the office or at home without the need for additional hardware,” said Carl Pinto, vicemore...

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter