Press Release Search

all Press Releases

  • 6/14/11 8:01 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today introduced the CAMILEO™ P100 and CAMILEO B10, two highly affordable and ultraportable 1080p full HD camcorders. Compatible with Windows®-based and Mac OS systems, both camcorders offer impressive zoom capabilities and double as 16-megapixel still cameras with dedicated recording buttons, enabling consumers to carry around a single device tomore...
  • 6/7/11 8:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today confirmed details around the upcoming launch of the Thrive™ Tablet, its first Android™-powered tablet for the U.S. market. Previously introduced as the “Toshiba Tablet,” the Thrive Tablet is set to deliver a more complete tablet experience by offering to consumers a tablet designed to deliver more performance, features and connectivitymore...
  • 4/20/11 6:34 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the launch of its waterproof CAMILEO® BW10 camcorder. The pocket-sized, HD camcorder comes in silver and yellow and features a rubberized coating that makes it perfect for recording underwater. The latest addition to Toshiba’s popular CAMILEO line, the BW10 camcorder offers versatility and resilience for consumers leading activemore...
  • 4/13/11 1:05 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba announces the first1 family of self-encrypting hard disk drives (HDDs) engineered to automatically invalidate protected data when connected to an unknown host. The new Toshiba Self-Encrypting Drive (SED) models enable OEMs to configure different data invalidation options that align with various end-user scenarios. Designed to address the increasing need for IT departments to comply with privacy laws andmore...
  • 4/12/11 8:01 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced its new range of high-performance business laptops. Reengineered from the ground up with thin, light and highly-durable designs, the new Tecra® and Portégé® laptops redefine mobility for business professional offering full performance and long battery life ratings in three form factors as well as a standard three-year limitedmore...
  • 3/28/11 9:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba, a leader in high performance 2.5-inch enterprise-class hard disk drive (HDDs) technologies, announces achievement of the highest levels of performance according to benchmark testing* conducted on equipment manufactured by Super Micro Computer, Inc. (NASDAQ: SMCI). The testing demonstrated that Toshiba’s MBF series drives provide superior read and write performance, seek time, and power efficiencymore...
  • 3/22/11 8:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the 14-inch USB-powered Mobile LCD Monitor, ideal for adding an additional screen to any Windows-based laptop computer at work, school, home or anywhere one uses a laptop. Featuring a 14-inch diagonal widescreen display1 with 1366x768 resolution, the Toshiba Mobile Monitor is equipped with the same LCD panel as amore...
  • 1/24/11 9:00 pm EST
    IRVINE, Calif.--(BUSINESS WIRE)--Extending its innovation in the 1.8” hard disk drive (HDD) category, Toshiba Storage Device Division announces the industry’s first 1.8” drives with low-insertion force (LIF) SATA (Serial ATA) connectors, enabling a 10% smaller footprint compared to standard 1.8” drives using microSATA connectors. Developed for use in multiple devices, including tablets, consumer electronics devices and external HDDs, the new MKxx39GSLmore...
  • 1/6/11 9:00 am EST
    LAS VEGAS--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced its most advanced 3D LED TVs for 2011. Featuring exclusive CEVO Engine Technology that includes enhancements for 3D picture quality, the new LED TVs also boast new ultra-thin cosmetic designs with chrome trim that add a touch of elegance to any home décor. In addition, Toshiba plans to demonstrate its cutting edge Glasses Free 3Dmore...
  • 1/6/11 9:00 am EST
    LAS VEGAS--(BUSINESS WIRE)--CES 2011, LVCC Central Hall Booth #11026—Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced its most diverse lineup of televisions and digital video products. From vivid LCDs, to stunning LEDs and cutting-edge 3D TVs, plus TV/DVD combos in sizes and prices that fit any room or budget, Toshiba has something for everyone. 2011 Toshiba Flat Panel TV Lineup 3D TVsmore...

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter