Press Release Search

all Press Releases

  • 1/5/11 8:00 am EST
    LAS VEGAS--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced select Satellite® C655D laptop models will feature AMD’s new E-Series Accelerated Processing Unit (APU) with on-die graphics1. Designed with price conscious buyers in mind, the new Satellite C655D delivers enhanced media performance and an improved battery life rating while maintaining strong value-pricing. “Themore...
  • 1/5/11 8:00 am EST
    LAS VEGAS--(BUSINESS WIRE)--CES 2011, LVCC Central Hall Booth #11026 — Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the CAMILEO™ S30 camcorder, a new addition to the highly acclaimed CAMILEO S-Series line. Toshiba’s latest lightweight and ultraportable full HD resolution camcorder now features image stabilization in 1080p1, 720p and 480p modes for smooth and clear videos, a touch screen designed for easiermore...
  • 1/5/11 8:00 am EST
    LAS VEGAS--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced its newest netbooks built for comfort, including the all new mini NB505 and an update to the award-winning mini NB305, featuring enhanced styling and performance. Toshiba’s award-winning netbooks consistently feature premium designs and are hallmarked by comfort-driven, full-sized keyboards, large touch pad and aremore...
  • 12/13/10 9:00 pm EST
    IRVINE, Calif.--(BUSINESS WIRE)--Extending its position in the enterprise storage market, Toshiba Storage Device Division announces its new family of enterprise-class solid state drives (SSDs). Developed to meet the market’s demand for higher performance and lower power consumption, the new MKx001GRZB series combines Toshiba hard disk drive (HDD) expertise and its leadership as the inventor of NAND flash technology. The 2.5-inch small form factormore...
  • 11/30/10 9:10 am EST
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba Storage Device Division (SDD), the pioneer in small form factor hard disk drives (HDDs), today announced a 7,200 RPM 2.5-inch Self-Encrypting Drive (SED) that provides government-grade AES-256 hardware encryption incorporated in the disk drive’s controller electronics. Based on the Opal Security Subsystem Class (Opal SSC) specification from the Trusted Computing Group (TCG), the new Toshiba SED enables securemore...
  • 11/15/10 9:00 pm EST
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba Storage Device Division (SDD), the pioneer in small form factor hard disk drives (HDDs), today announced two new 2.5-inch HDD models designed for rugged 24-hour continuous operation in computing, industrial, and other extreme environments. The new models – the 100GB1 SATA interface MK1060GSCX and the 80GB1 PATA interface MK8050GACY – offer exceptional reliability and performance across wide temperature, altitudemore...
  • 10/12/10 3:04 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today introduced two 4G WiMAX-ready1 models of the Portégé® R700, the world’s lightest 13.3-inch full-performance ultraportable laptop with an integrated DVD drive2. The new Portégé R700 models not only provide business users with unprecedented performance and durability in a highly mobile form factor, but the most comprehensive connectivitymore...
  • 9/28/10 6:08 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba's Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today introduced Toshiba Book Place, an e-book reader and store that adds easy-to-access, interactive e-books to the suite of digital entertainment products that consumers can enjoy on laptops. In partnership with K-NFB Reading Technology, Inc., a joint venture between Kurzweil Technologies Inc. and the National Federation for the Blind, Toshibamore...
  • 9/28/10 2:45 pm EDT
    IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced that it has added powerful new features to enhance the 3D playback capabilities of its Satellite® A665-3D Series laptops. Equipped with NVIDIA® 3D Vision™ technology1, the updated laptop models are ready to deliver a stereoscopic 3D experience to games, movies, photos and more. New features further enhance the experience, givingmore...
  • 9/28/10 9:00 am EDT
    IRVINE, Calif.--(BUSINESS WIRE)--With the ever-increasing demands of digital media, Toshiba introduces the Canvio™ 3.0 portable hard disk drive (HDD) featuring a SuperSpeed USB 3.0 interface. For the same price as competing USB 2.0 drives, Canvio 3.0 drives offer blazing fast file transfers at up to 10 times the speed of USB 2.0 drives. Available in storage capacities of 500 gigabytes (GB1), 750GB or one terabyte (TB1), Canvio 3.0 drives feature simplemore...

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter