The Power of Two: Toshiba Announces Ultra-Compact Satellite Click 10 Detachable 2-in-1 PC

Designed for Windows 10, 2-in-1 PC features 10.1-inch Full HD Touchscreen and Latest Intel Processor with Lightning Fast Performance and Outstanding Battery Life

Tuesday, September 15, 2015 8:00 am EDT

Dateline:

IRVINE, Calif.
"Committed to People, Committed to the Future"

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced an all-new ultra-compact 2-in-1 detachable PC, the Satellite Click™ 10. Measuring 30 percent smaller and 50 percent lighter than a typical laptop1, the Satellite Click 10 offers the versatility of a slim tablet plus a lightweight laptop in one easy-to-carry device, weighing just 2.2 pounds with the full-size keyboard attached2.

“We’ve created a highly portable, versatile PC that can move easily from laptop productivity to tablet fun,” said Philip Osako, senior director of product marketing, Toshiba America Information Systems, Inc., Digital Products Division. “With a stunning Full HD display that easily detaches as a tablet, plus exclusive features that enhance the Windows 10 experience, this device is perfect for someone always on the go.”

The Satellite Click 10 features a brilliant 10.1-inch diagonal 1900 x 1200 resolution TruBrite® multi-touch display3 that supports Full HD 1080p content, delivering excellent color and contrast for watching, playing, working and more. The display can be easily detached and used as a tablet that measures only 0.36 inches thin and weighs just 1.2 pounds.

Designed for Windows 10

The Satellite Click 10 is designed to enhance the new features and capabilities of Windows 10. For voice apps like Cortana4 and Skype, the Satellite Click 10 features multi-directional TruTalk™ microphones, a dedicated Cortana key for easily calling up Microsoft’s personal digital assistant plus a high-resolution 8MP rear camera and 2MP front webcam for video chatting and taking photos. In addition, the device comes with Office mobile apps pre-installed, enabling users to get productive right out of the box, in both laptop and tablet modes.

Impressive Performance for Productivity on the Go

The Satellite Click 10 is powered by the new Intel® Atom™ x5 processor with 64-bit processing5. This latest processor from Intel provides all the performance, agility and speed for a rich mobile experience, including editing photos and videos, making changes to presentations on the go, and switching quickly between apps, while delivering a battery life rating of more than seven hours6. To make the most of entertainment, the Satellite Click 10 includes stereo speakers with Dolby Digital Plus™.

The tablet is equipped with a Micro HDMI® port for sharing the display with a large-screen HDTV or external display, a microSD™ card slot to expand the storage or transfer files and can be configured with 32GB or 64GB flash storage7 and 2GB of RAM8. The keyboard dock includes two USB 2.0 ports for easy sync and share with smartphones and other USB-powered gadgets.

Exclusive Apps Designed for the Way You Work

To help users make the most of the device, the Satellite Click 10 includes Toshiba’s exclusive suite of Tru apps, with apps designed to enhance the camera and sound recording capabilities, making it easier to capture detailed notes from whiteboards, textbooks, meetings and more.

Pricing and Availability

The Satellite Click 10 is now available for pre-order at select online retailers and direct from Toshiba on toshiba.com/us, starting at $349.99 MSRP9.

Image Gallery: http://bit.ly/SatelliteClick10

Connect with Toshiba on Facebook at www.facebook.com/ToshibaUSA, on Twitter at twitter.com/ToshibaUSA, and on YouTube at youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of five business units: Business Solutions Division, Digital Products Division, Imaging Systems Division, Telecommunication Systems Division and Industrial Solutions & Services Division. Together, these divisions provide digital products, services and solutions, including award-winning notebook computers, tablets, branded storage products, digital display solutions, cloud services; imaging products for the security, medical and manufacturing markets; IP business telephone systems with unified communications, collaboration and mobility applications; and IoT solution development, data analytics and IT services. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation, a Fortune Global 500 company, channels world-class capabilities in advanced electronic and electrical product and systems into five strategic business domains: Energy & Infrastructure, Community Solutions, Healthcare Systems & Services, Electronic Devices & Components, and Lifestyles Products & Services. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations and is contributing to the .realization of a world where generations to come can live better lives.

Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global network of over 580 consolidated companies employing 199,000 people worldwide, with annual sales surpassing 6.6 trillion yen (US$55 billion). To find out more about Toshiba, visit www.toshiba.co.jp/index.htm.

© 2015 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

1 Weight/size claim based on Toshiba 15” Satellite laptop

2 Weight. Weight may vary. See Weight Legal Footnote at www.info.toshiba.com

3 Display. Any small bright dots that may appear on your display are an intrinsic characteristic of the thin film transistors manufacturing technology. See Display Legal Footnote at www.info.toshiba.com

4 Availability of Cortana is dependent on market, experience varies by market

5 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com

6 Battery Life Rating. Measured by MobileMark® 2014 for comparison purposes only. Actual battery life may vary. See Battery Life Rating Legal Footnote at www.info.toshiba.com

7 Solid State Drive Capacity. Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Solid State Drive Capacity Legal Footnote at www.info.toshiba.com

8 Memory. Memory size may vary. See Memory Legal Footnote at www.info.toshiba.com

9 Price. Reseller prices may vary. MSRP means “Manufacturer’s Suggested Retail Price.”

Contact:

Access Communications
Yulimar Chiu, 415-844-6240
ychiu@accesspr.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter