Toshiba Adds 4G WiMAX Capabilities to Award-winning Portégé R700

Tuesday, October 12, 2010 3:04 pm EDT

Dateline:

IRVINE, Calif.
"4G WiMAX coverage continues to rapidly grow and offers millions of people wireless access in many major metropolitan areas across the U.S."

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today introduced two 4G WiMAX-ready1 models of the Portégé® R700, the world’s lightest 13.3-inch full-performance ultraportable laptop with an integrated DVD drive2. The new Portégé R700 models not only provide business users with unprecedented performance and durability in a highly mobile form factor, but the most comprehensive connectivity options available.

“4G WiMAX coverage continues to rapidly grow and offers millions of people wireless access in many major metropolitan areas across the U.S.,” said Carl Pinto, vice president of product development, Toshiba America Information Systems, Inc., Digital Products Division. “Now with a WiMAX-enabled Portégé R700, Toshiba business professionals will be able to enjoy the benefits of having citywide connectivity at their fingertips.”

WiMAX is currently available in 54 cities nationwide and is expected to be available in Cincinnati, Cleveland, Denver, Los Angeles, San Francisco, Miami, Minneapolis, New York and Pittsburgh by the end of 2010.

With a starting weight of just three pounds3 and about one inch thin, the Portégé R700 supports the latest Intel® Core™ family of full-powered processors and a wealth of features and ports required by business users, including the ability to dock to a port replicator, an ExpressCard™ slot, an eSATA/USB combo port with Sleep-and-Charge4, as well as a built-in DVD SuperMulti drive and Webcam. The Portégé R700 also features a high-capacity six-cell battery with a long battery life rating5.

The Portégé R700-S1332W features the Intel Core i7 processor6 and a 128GB solid state drive7, while the Portégé R700-S1322W features the Intel Core i5 processor and a 320GB high-speed 7200 RPM hard drive8. Both include 4GB of DDR3 memory9.

With a light, yet durable magnesium alloy casing reinforced with a honeycomb rib design, the Portégé R700 features a 13.3-inch diagonal HD widescreen LED-backlit display10, a premium raised tile keyboard and a wide TouchPad™ with customizable Multi-touch Control that makes typing and navigation easy and comfortable.

Availability

The WiMAX-enabled Portégé R700-S1332W ($1,699 MSRP11) and Portégé R700-S1322W ($1,349 MSRP) will be available on Oct. 12, 2010 through select Toshiba Preferred Partner Program resellers and e-tailers.

Image Gallery: http://bit.ly/PortegeR700

Connect with Toshiba on Twitter at twitter.com/ToshibaLaptops and on Facebook at www.facebook.com/ToshibaLaptopsUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of four business units: Digital Products Division, Imaging Systems Division, Storage Device Division, and Telecommunication Systems Division. Together, these divisions provide mobile products and solutions, including industry-leading portable computers; televisions, TV/DVD Combination products, Blu-ray Disc and DVD products, and portable devices; imaging products for the security, medical and manufacturing markets; storage products for automotive, computer and consumer electronics applications; and IP business telephone systems with unified communications, collaboration and mobility applications. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America.

TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. Toshiba Corporation is a world leader and innovator in high technology, a diversified manufacturer and marketer of advanced electronic and electrical products. These products span from information & communications systems; digital consumer products; electronic devices and components; as well as power systems including nuclear energy; industrial and social infrastructure systems; and home appliances. Toshiba was founded in 1875, and today operates a global network of more than 740 companies, with 204,000 employees worldwide and annual sales surpassing $68 billion (6.3 Trillion Yen). For more information on Toshiba visit www.toshiba.com.

© 2010 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

1 WiMAX™ wireless use requires separately purchased subscription service. Access limited to coverage area.

2 As of June 21, 2010.

3 Weight. Weight may vary. See Weight Legal Footnote at www.info.toshiba.com

4 The "USB Sleep & Charge function" may not work with certain external devices even if they are compliant with the USB specification. In those cases, turn the power of the computer ON to charge the device.

5 Battery Life Rating. Measured by MobileMark® Productivity 2007 for comparison purposes only. Actual battery life may vary. See Battery Life Rating Legal Footnote at www.info.toshiba.com

6 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com

7 Solid State Drive Capacity. Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Solid State Drive Capacity Legal Footnote at www.info.toshiba.com

8 Hard Disk Drive Capacity. Hard drive capacity may vary. 1 Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Hard Disk Drive Capacity Legal Footnote at www.info.toshiba.com

9 Memory. Memory size may vary. See Memory Legal Footnote at www.info.toshiba.com

10 Display. Any small bright dots that may appear on your display are an intrinsic characteristic of the thin film transistors manufacturing technology. See Display Legal Footnote at www.info.toshiba.com

11 Price. Reseller prices may vary. MSRP means "Manufacturer's Suggested Retail Price."

Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=6465046&lang=en

Multimedia Files:

Preview image
Toshiba today introduced two 4G WiMAX-ready models of the Portege R700, the world's lightest 13.3-inch full-performance ultraportable laptop with an integrated DVD drive. (Photo: Business Wire)

Contact:

Access Communications
Jared Leavitt, 415-844-6253
jleavitt@accesspr.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter

  • Early childhood education is a critical time in a person's development . Here's how you can use science to inform… https://t.co/jEhSBPGSsu1 day 11 hours ago
  • The internet has provided this generation of students with access to an unparalleled amount of information .… https://t.co/lG9CepzXcu1 day 14 hours ago
  • 3D printers are an engaging way to get students involved in . Congrats to Mrs. Garntner from Jen… https://t.co/fYqi95IupJ2 days 12 hours ago
  • Early can foster a lifelong love of science and mathematics in young learners . Here’s why it is crucial t… https://t.co/hn1rEgsDNh2 days 13 hours ago