Toshiba Adds 6th Generation Intel Processors to Enterprise-Class Z Series Mobile Solutions

Complete Enterprise PC Portfolio Features, Full HD Screens, and a Range of Security, Productivity and Manageability Capabilities

Tuesday, January 26, 2016 9:00 am EST

Dateline:

IRVINE, Calif.
"Committed to People, Committed to the Future"

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Business Solutions Division (BSD), a division of Toshiba America Information Systems, Inc., today announced the addition of the 6th Generation Intel® Core™ processors to its line of high-performance, enterprise-class of thin-and-light mobile computing devices.

This lineup consists of a 13.3-inch Portégé® Z30 and 14-inch Tecra® Z40 Ultrabooks™, which come with a variety of screen options. The award-winning Portégé Z20t Detachable 2-in-1 Ultrabook now features the new USB Type-C™ reversible connector to increase data speeds. Rounding out the portfolio is the 15.6-inch Tecra Z50, which features an entirely new aluminum chassis.

“By extending the capabilities, performance and bandwidth of our updated enterprise line of Portégé and Tecra products, we’re giving mobile professionals a better way to work,” said Carl Pinto, vice president of marketing and engineering, Toshiba America Information Systems, Inc., Digital Products Division. “With the new Intel ‘Skylake’ processors included in our lineup, enterprise customers will enjoy increased form factor performance, reliability, advanced security and impressive craftsmanship they’ve come to expect from Toshiba for the past three decades.”

Performance and Features for Greater Productivity On-the-Go

Powered by 6th Generation Intel Core processors, the 13.3-inch Portégé Z30 and 14-inch Tecra Z40 Ultrabooks feature HD, Full HD, and Full HD touch-enabled displays offering plenty of screen real estate to work. With superior performance, extended battery life and enhanced durability, as well as a full array of security features, essential ports, and a variety of storage technology options, the thin-and-light Portégé Z30 and Tecra Z40 Ultrabooks serve as ultimate work machines that also deliver on mobility and style.

The powerful and durable Tecra Z50 laptops deliver everything today’s mobile workers need in a desktop replacement. The 15.6-inch Tecra Z50 features a 6th Generation Intel Core processor and a brand new design with aluminum chassis without compromising on essential business features like manageability, security and connectivity.

Also featuring the latest Intel processors, the versatile Portégé Z20t Detachable 2-in-1 Ultrabook delivers the enhanced speed and performance expected from a business-class Portégé device and allows users to switch instantly between notebook and tablet by simply detaching the screen. Equipped with all of the business-essential ports needed for a dongle-free experience and a 12.5-inch diagonal Full HD anti-glare touchscreen display, the Portégé Z20t is an ideal choice for on-the-go professionals looking for a single, multifunctional device that offers more screen real estate than most tablets and the responsive performance of a laptop. The Portégé Z20t now features the new USB Type-C connector, which allows reversible use and increases data speeds.

Common Docking and Accessories

The new 13.3-, 14- and 15.6-inch laptops share a common docking port and accessories, including power adapters and port replicators, making it easier for IT managers to purchase, deploy and manage these devices for their companies. Additionally, they also share a common image, allowing IT departments to easily customize their machines to meet unique needs across the company and deploy them to users in an efficient manner.

Save Time and Money with Toshiba’s Configuration Services

Regardless of how many laptops are purchased at one time, Toshiba can perform the most tedious configuration tasks before delivery, saving tremendous time for overburdened IT departments. Our Configuration-to-Order (CTO) services, performed in our own Toshiba factories, include image build, load and certification; custom asset tagging; company logo etching; individualized BIOS settings; provisioning; Absolute Computrace® factory activation and more. Toshiba ensures that each device arrives exactly as you want it with no additional work required, allowing your IT staff to focus on more strategic tasks.

Additionally, with Toshiba’s Build-to-Order (BTO) services, organizations can receive laptops built to their exact specifications to ensure high efficiency and proper workflow for a variety of enterprise needs. Toshiba offers the ability to choose from a variety of processors, storage and memory capacities, and display options to offer enterprise employees a device best equipped for day-to-day operations.

Windows Operating System Flexibility

Toshiba’s enterprise portfolio of notebooks will feature a variety of Microsoft® operating systems to best suit each organization's IT requirements, including Windows 10 and Windows 7 with Microsoft Windows 10 upgrade licensing rights.

Better Manageability for IT with Toshiba Smart Client Manager

The Tecra and Portégé laptops are the perfect platform for the Toshiba Cloud Client Manager (TCCM) – a cloud service that allows IT administrators to easily manage end-point devices across a deployment by providing comprehensive tools and patch management to ensure device efficiency and compliance. Using a standard web browser, IT administrators can now oversee and take control of devices online, in real-time, without the need to invest in servers and dedicated management software. The devices also have advanced manageability options, supporting Microsoft System Center Configuration Manager (SCCM), Windows® Management Instrumentation (WMI) and Toshiba Smart Client Manager 2.0 (TSCM).

Toshiba BIOS for more efficient (and secure) asset management

With Toshiba’s proprietary BIOS, Tecra® laptops deliver seamless integration of hardware and software that few PC manufacturers can deliver. Having proprietary BIOS speeds laptop customization and saves time managing assets—a valuable benefit for companies with limited IT resources. This foundational BIOS software also monitors the PC’s internal components to maintain stability, while offering system-level security and built-in countermeasures to prevent unauthorized access.

Pricing and Availability

The Portégé Z20t, Portégé Z30t, Tecra Z40t, and Tecra Z50 are all available for purchase through our network of resellers as well as Corporate Direct and our strategic partners: CDW, PC Connections, PCM, Insight, SHI and Zones.

The Portégé Z20t Detachable Ultrabooks starts at $999.99 MSRP.

The Portégé Z30 Ultrabooks start at $1,279.99 MSRP.

The Tecra Z40 Ultrabooks starts at $1,229.99 MSRP.

The Tecra Z50 laptops start at $1,599.99 MSRP.

Image Gallery: http://bit.ly/2016Q1-Enterprise

Connect with Toshiba Business Solutions Division on LinkedIn at https://www.linkedin.com/company/toshiba, on Twitter at twitter.com/ToshibaUSA, on Facebook at www.facebook.com/ToshibaUSA and on YouTube at youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of four business units: Business Solutions Division, Digital Products Division, Imaging Systems Division, and Telecommunication Systems Division. Together, these divisions provide digital products, services and solutions, including industry-leading notebook computers, tablets and All-in-One computers, televisions, TV/DVD Combination products, Blu-ray Disc™, DVD players and media boxes, as well as cloud services; imaging products for the security, medical and manufacturing markets; storage products for computers; and IP business telephone systems with unified communications, collaboration and mobility applications. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation, a Fortune 500 company, channels world-class capabilities in advanced electronic and electrical product and systems into five strategic business domains: Energy & Infrastructure, Community Solutions, Healthcare Systems & Services, Electronic Devices & Components, and Lifestyles Products & Services. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations towards securing “Growth Through Creativity and Innovation”, and is contributing to the achievement of a world in which people everywhere live in safe, secure and comfortable society. Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide, with annual sales surpassing 6.5 trillion yen (US$63 billion). To find out more about Toshiba, visit www.toshiba.co.jp/index.htm

© 2016 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

Contact:

Access Communications
Kaylin Slakey, 415-844-6234
kslakey@accesspr.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter