Toshiba Expands SMB Offerings Backed by a Unique Replacement Guarantee

Built with Intel Core Processor Technology, New 15.6-inch, 14-inch and 13.3-inch Tecra® and Portégé® Laptops Deliver Enterprise-class Performance and Durability at Affordable Price Points

Tuesday, January 26, 2016 9:00 am EST

Dateline:

IRVINE, Calif.
"Committed to People, Committed to the Future"

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Business Solutions Division (BSD), a division of Toshiba America Information Systems, Inc., today announced several new laptops designed to meet the varying needs of small businesses and mid-sized organizations. Designed, engineered and manufactured by Toshiba, the 14-inch Tecra C40 and Tecra A40, the 13.3-inch Portégé A30, the 15.6-inch Tecra A50, and the refreshed 15.6-inch Tecra C50 represent the expansion of Toshiba’s SMB lineup to include more choices in form factors, security and docking capabilities. The C Series laptops and the step-up A Series laptops are powered by Intel 6th generation core processors, while the entry-level Tecra C50 is powered by an Intel 5th generation core processor. All of the notebooks include Toshiba’s Quality Replacement Guarantee to increase peace of mind in making an investment in Toshiba.

“Small businesses and mid-sized organizations have many needs and varying preferences when it comes to their devices but often have fewer choices compared to their large enterprise counterparts,” said Carl Pinto, vice president of marketing and engineering, Toshiba America Information Systems, Inc., Business Solutions Division. “With our expanded line of Tecra and Portégé products, we are able to offer a wide range of options to enhance user productivity, while delivering devices with enterprise-class performance for a low total cost of ownership.”

Big Performance for Small Business

The entry-level C series laptops feature essential ports, HD displays and Intel processors1. The laptops also feature a built-in DVD Drive2 as well as user-replaceable batteries.

The higher-end A Series laptops are equipped with a docking port and utilize the High Speed Port Replicator that is common across Toshiba’s Tecra and Portégé® line. The A Series notebooks also include a state-of-the-art Fingerprint Reader, spill-resistant, full-size backlit keyboard and Accupoint® pointing system.

The Tecra C50 and A50 feature a full-size keyboard with a 10-key numeric pad for easily powering through spreadsheets.

Toshiba Quality Replacement Guarantee

To demonstrate its commitment to quality and reliability, Toshiba is including the Toshiba Quality Replacement Guarantee3 for these new laptops. If the LCD panel, hard drive, memory or system board fails within the first year of ownership, Toshiba will replace the unit with a new laptop.

Excellent Battery Life Rating

Toshiba’s SMB laptops boast long lasting batteries to allow users the flexibility to tackle business tasks without interruption wherever business might happen. All models include a user-replaceable battery for greater convenience and assurance of laptop longevity.

Windows Operating System Flexibility

With its new line of SMB devices, Toshiba will offer a variety of Microsoft® operating systems to best suit each organization's IT requirements. Each device will ship with Microsoft’s Windows 7 operating system, and will include Microsoft Windows 10 upgrade licensing rights in the packaging.

Toshiba BIOS for More Efficient (and Secure) Asset Management

With Toshiba’s proprietary BIOS, both Tecra and Portégé laptops deliver seamless integration of hardware and software that few PC manufacturers can deliver. Having proprietary BIOS speeds laptop customization and saves time managing assets—a valuable benefit for companies with limited IT resources. This foundational BIOS software also monitors the PC’s internal components to maintain stability, while offering system-level security and built-in countermeasures to prevent unauthorized access.

Efficient Collaboration and Sharing

To make the process of connecting, syncing, sharing and collaborating easier, the laptops are equipped with a webcam, Bluetooth® v4.0, the latest dual-band 802.11ac + abgn Wi-Fi®, and are wireless display ready4. A generous range of essential ports make doing business easier, including USB 3.05 and USB 2.0 ports, plus full-size HDMI® and VGA ports, Gigabit Ethernet and an SD Card reader. The line of dongle-free devices include a built in ODD and a user replaceable battery.

Easy to Manage within Corporate IT Environments

Toshiba developed the Tecra and Portégé laptops as the perfect complement platforms for the Toshiba Cloud Client Manager (TCCM) – a cloud service that allows IT administrators to easily manage end-point devices across a deployment by providing comprehensive tools and patch management to ensure device efficiency and compliance. Using a standard web browser, IT administrators can now oversee and take control of devices online in real-time.

EasyGuard Technology

In addition to a spill resistant keyboard designed and tested to help save data and shut down, these laptops all feature Toshiba’s innovative EasyGuard® Technology, adding multi-tiered security and data protection measures that guard components against accidental bumps. For quality and reliability, the laptops are rigorously tested to the stresses of heat, shock, vibration and Highly Accelerated Life Testing (HALT) at Toshiba’s facilities.

Pricing and Availability

Toshiba notebooks are available from our network of resellers as well as our strategic partners: CDW, PC Connections, PCM, Insight, SHI and Zones. Pricing for the C Series starts at $545.99 and $829.99 for the A Series.

Image Gallery: http://bit.ly/2016Q1-SMB

Connect with Toshiba Business Solutions Division on LinkedIn at https://www.linkedin.com/company/toshiba, on Twitter at twitter.com/ToshibaUSA, on Facebook at www.facebook.com/ToshibaUSA and on YouTube at youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of four business units: Business Solutions Division, Digital Products Division, Imaging Systems Division, and Telecommunication Systems Division. Together, these divisions provide digital products, services and solutions, including industry-leading notebook computers, tablets and All-in-One computers, televisions, TV/DVD Combination products, Blu-ray Disc™, DVD players and media boxes, as well as cloud services; imaging products for the security, medical and manufacturing markets; storage products for computers; and IP business telephone systems with unified communications, collaboration and mobility applications. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation, a Fortune 500 company, channels world-class capabilities in advanced electronic and electrical product and systems into five strategic business domains: Energy & Infrastructure, Community Solutions, Healthcare Systems & Services, Electronic Devices & Components, and Lifestyles Products & Services. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations towards securing “Growth Through Creativity and Innovation”, and is contributing to the achievement of a world in which people everywhere live in safe, secure and comfortable society. Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide, with annual sales surpassing 6.5 trillion yen (US$63 billion). To find out more about Toshiba, visit www.toshiba.co.jp/index.htm

© 2016 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

1 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com#ProcessorCentralProcessingUnit

2 Copy protection technology may prevent or limit recording or viewing of certain optical media (e.g., CD or DVD).

3 Toshiba Quality Guarantee. Cosmetic damage due to handling and wear of the product is not included in this program, including keyboards, case work covers, key caps and plastic pieces. All of Toshiba’s standard limited warranty terms and limitations apply.

4 Wireless. May require purchase of additional software, external hardware, or services. Transmission speeds may vary. Certain optional features within the wireless-n specifications (if available on your system) may not be supported.

5 5Gbps is the maximum theoretical interface transfer rate per the specifications of the Universal Serial Bus 3.0. Actual transfer rate will vary depending on your system configuration and other factors.

Contact:

Access Communications
Kaylin Slakey, 415-844-6234
kslakey@accesspr.com

Connect with Toshiba

Presentations & Reports

Toshiba on Twitter