New Satellite T100 Series Laptops Feature Power-Efficient AMD Turion X2 Neo, Athlon X2 Neo and Athlon Neo MV-40 Processors, Delivering Broader Range of Multimedia Capabilities in Ultrathin Category
CES 2010, LVCC Central Hall Booth #12114
Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today expanded its line of Satellite® T100 Series ultra-thin laptops to include models equipped with processors from AMD, delivering enhanced multimedia processing power to the ultra-thin category.
Satellite T100 Series laptops are designed for those looking for a stylish ultra-thin form factor that delivers a balance of performance, features and affordability needed for everyday mobility. New configurations based on the AMD Neo™ platform deliver the versatility of dual-core processor performance, plus ATI Radeon™ graphics that enhance the laptop’s multimedia prowess.
“The emergence of the low-cost ultra-thin category has quickly proven that consumers do not need to give up performance for mobility,” said Carl Pinto, vice president of product development, Toshiba America Information Systems, Inc., Digital Products Division. “The Satellite T100 series provide the right blend of features with the right form factor to meet a broad set of computing needs.”
At less than one-inch thin and weighing under four pounds, Satellite T100 Series laptops are topped with a stylish Fusion™ Finish and feature comfortable full-size keyboards and TouchPads™ with Multi-touch Control. Designed for mobility, the laptops include a Hard Drive Impact Sensor that helps guard data from the daily bumps of mobile life and a USB port with Sleep-and-Charge1 technology, which enables users to charge various consumer electronics, even when the laptop is turned off. A built-in Webcam with Face Recognition2 makes logging in hassle-free and live chat possible from anywhere, and a standard one-year limited international warranty3 makes traveling more worry-free. The Satellite T100 Series laptops also feature fast resume functionality so they are ready when needed – up and running in seconds.
Equipped with Windows® 7 Home Premium, spacious hard drives up to 320GB4, up to 4GB of memory5 and lots of expansion ports, including HDMI output, the laptops have the horsepower to handle everyday computing, Web and digital entertainment needs. Select models include built-in Wireless-N Wi-Fi6 technology and Bluetooth®6 (on select models) provides users with the latest in connectivity technology to keep users productive, online and in touch.
The new Satellite T100 Series laptops with AMD processors will be available in two screen sizes and various color options. Designed to be stylish both inside and out, Toshiba’s Fusion Finish design extends inside the laptop, around the keyboard, touch pad and the display. The Satellite T135D features a 13.3-inch diagonal LED backlit widescreen display and will be available in Nova Black, Red and White, while the Satellite T115D offers an 11.6-inch diagonal widescreen LED backlit display and will be available in Nova Black.
New Multimedia Software Built for Digital Entertainment
The new Satellite T100 Series laptops will come pre-installed with the recently announced Toshiba Media Controller™7 software, a new application that makes it easier to share content across a home network. The Toshiba Media Controller application enables users to effortlessly share files, photos and stream music and video across a wireless network between other Windows PCs and Windows 7-compatible devices, such as the Xbox® 360 game console through a simple drag-and-drop interface.
The laptops will also include Toshiba’s ReelTime™ and Bulletin Board™ apps, which give consumers an enhanced experience when accessing files, organizing daily activities, managing projects and more – right from their desktops.
EPEAT Gold-rated Eco-conscious Design
The Satellite T135D and Satellite T115D laptops are designed to be environmentally conscious with power-efficient, mercury-free LED backlit displays and meet the rigorous requirements of the EnergyStar® 5.0 standard, and achieved industry-leading Electronic Product Environmental Assessment Tool (EPEAT®) Gold status. They are also RoHS compatible, effectively reducing the environmental impact by restricting the use of lead, mercury, cadmium and certain other hazardous substances.
Features available on the Toshiba Satellite T135D laptop include:
- 13.3-inch diagonal widescreen HD TruBrite™ LED Backlit display
- Windows® 7 Home Premium operating system (64-bit)
- AMD Turion™ Neo X2, Athlon™ Neo X2 or Athlon Neo MV-40 processor8
- ATI Radeon™ 3200 graphics (on select models)9
- Up to 4GB DDR2 RAM5
- Up to 320GB (5400 RPM) HDD4
- 802.11b/g/n wireless6 and 10/100 Ethernet
- Bluetooth® V2.1 + EDR (available on select models)6
- Toshiba Hard Drive Impact Sensor
- TouchPad™ with Multi-touch Control
- Lightweight at only 3.88 lbs.
- Long-life 6-cell battery delivering battery life rating up to 6 hours, 13 minutes10
- One eSATA/USB combo port with USB Sleep-and-Charge1 and two USB 2.0 ports
- HDMI port
- Built-in Webcam with Toshiba Face Recognition, stereo speakers and microphone
- 5-in-1 Memory Card Reader Slot
- Toshiba Media Controller™
- Toshiba Bulletin Board™
- Toshiba ReelTime™
- Toshiba PC Health Monitor
- Toshiba Online Backup
Features available on the Toshiba Satellite T115D laptop include:
- 11.6-inch diagonal widescreen HD TruBrite™ LED Backlit display
- Windows 7 Home Premium operating system (64-bit)
- AMD Athlon Neo X2 or Athlon Neo MV-40 processor8
- ATI Radeon 3200 graphics (on select models)9
- 2GB DDR2 RAM5
- 250GB (5400 RPM) HDD4
- 802.11b/g/n wireless6 and 10/100 Ethernet
- Bluetooth V2.1 + EDR (available on select models)6
- Toshiba Hard Drive Impact Sensor
- TouchPad with Multi-touch Control
- Lightweight at only 3.49 lbs.
- Long-life 6-cell battery delivering battery life rating up to 5.5 hours10
- One eSATA/USB combo port with USB Sleep-and-Charge1 and two USB 2.0 ports
- HDMI port
- Built-in Webcam with Toshiba Face Recognition, stereo speakers and microphone
- 5-in-1 Memory Card Reader Slot
- Toshiba Media Controller
- Toshiba Bulletin Board
- Toshiba ReelTime
- Toshiba PC Health Monitor
- Toshiba Online Backup
Pricing and Availability
The Satellite T135D (starting at $599.99 MSRP11) and Satellite T115D (starting at $449.99 MSRP11) laptops will be available on January 17 at major retailers, e-tailers and direct from Toshiba on toshibadirect.com.
More information and detailed specifications about the Satellite T100 Series can be found at laptops.toshiba.com/laptops/satellite/T100.
Image Gallery: http://bit.ly/satelliteT100
Connect with Toshiba on Twitter at twitter.com/ToshibaLaptops and on Facebook at www.facebook.com/ToshibaLaptopsUS.
About Toshiba America Information Systems Inc. (TAIS)
Headquartered in Irvine, Calif., TAIS is comprised of four business units: Digital Products Division, Imaging Systems Division, Storage Device Division, and Telecommunication Systems Division. Together, these divisions provide mobile products and solutions, including industry leading portable computers; projectors; imaging products for the security, medical and manufacturing markets; storage products for automotive, computer and consumer electronics applications; and telephony equipment and associated applications.
TAIS provides sales, marketing and services for its wide range of information products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. Toshiba Corporation is a world leader and innovator in high technology, a diversified manufacturer and marketer of advanced electronic and electrical products. These products span from information & communications systems; digital consumer products; electronic devices and components; as well as power systems including nuclear energy; industrial and social infrastructure systems; and home appliances. Toshiba was founded in 1875, and today operates a global network of more than 730 companies, with 199,000 employees worldwide and annual sales surpassing US$67 billion. For more information on Toshiba visit toshiba.com.
© 2010 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.
1 USB Sleep & Charge. The "USB Sleep & Charge function" may not work with certain external devices even if they are compliant with the USB specification. In those cases, turn the power of the computer ON to charge the device.
2 Toshiba Face Recognition. For high security purposes, Toshiba Face Recognition is not a suitable substitute for Windows® passwords. To ensure the security of your system use your established Windows® passwords to logon.
3 Warranty. The terms and conditions of Toshiba's standard limited warranty, and extended warranty and service upgrade plans are available at www.warranty.toshiba.com.
4 Hard Disk Drive Capacity. Hard drive capacity may vary. 1 Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Hard Disk Drive Capacity Legal Footnote at www.info.toshiba.com.
5 Memory. Memory size may vary. See Memory Legal Footnote at www.info.toshiba.com.
6 Wireless. May require purchase of additional software, external hardware, or services. Transmission speeds may vary. See Wireless Legal Footnote at www.info.toshiba.com.
7 Toshiba Media Controller. Copy protection technology, if any, associated with the content may prevent or limit sharing of content.
8 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com.
9 Graphics. GPU performance may vary. See Graphics Legal Footnote at www.info.toshiba.com.
10 Battery Life Rating. Measured by MobileMark® Productivity 2007 for comparison purposes only. Actual battery life may vary. See Battery Life Rating Legal Footnote at www.info.toshiba.com.
11 Price. Reseller prices may vary. MSRP means "Manufacturer's Suggested Retail Price."
Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=6132373&lang=en