View all news

Toshiba Unveils Portégé Z830 Series of Ultrabook Systems

09/01/2011

The World’s Lightest 13.3-inch Platform, Sub-2.5 Pound Portégé Z830 Series Match Style, Supreme Portability and Enhanced Functionality at Affordable Prices

Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today unveiled the Portégé® Z830 Series, the company’s first Ultrabook™ using 2nd Generation Intel® Core™ processors. Weighing less than 2.5 pounds1 and featuring a 0.63-inch (15.9 mm) profile, the Portégé Z830 Series is about 20 percent lighter and 40 percent thinner than the award-winning ultraportable Portégé R830 Series. These new systems offer unprecedented portability, durability and essential features with visibly smart style and responsiveness — and start at under $1,000 MSRP2.

Supporting the latest 2nd Generation Intel Core processors3 and ultra-fast DDR3 memory, the Portégé Z830 Series provides the performance needed for work and entertainment plus improved power management for great battery life. The Ultrabook device’s 128GB solid state drive4 delivers an extremely responsive experience, increased durability and increased energy efficiency. Paired with Toshiba’s new exclusive Hi-Speed Start Technology, the Portégé Z830 can power on and get users up and running at work or home in just seconds.

“The Portégé Z830 Series sets a new standard for thin and light systems, not just in portability, but also in affordability for such cutting-edge designs,” said Carl Pinto, vice president of product development, Toshiba America Information Systems, Inc., Digital Products Division. “Toshiba’s engineering achievements and expert craftsmanship have resulted in a brilliant and fully thought-through innovation that exceeds expectations, perfect for both mobile business professionals and consumers.”

The Portégé Z830 Series is built with a host of convenience-driven features such as a full-size LED Backlit and spill-resistant keyboard that makes typing easy in low light conditions and helps guard against accidents. The Ultrabook also includes Toshiba’s USB Sleep & Charge5 technology to give users the freedom to power up their smartphones even while the system is powered down. Stereo speakers with enhanced audio technology from Waves Audio make the Portégé Z830 ideal for listening to music, watching movies and video chatting.

The Ultrabook devices feature a light, yet durable magnesium alloy casing that is reinforced with an enhanced Honeycomb Rib design and new internal structures that provide shock absorption and increased rigidity. The systems also feature Toshiba’s EasyGuard® Technology, designed to address the security, reliability and durability issues mobile users encounter.

Availability

Portégé Z830 Series Ultrabook systems will be available in November 2011 at select retail stores as well as through select Toshiba Preferred Partner Program resellers and directly at toshibadirect.com.

Image Gallery: http://bit.ly/PortegeZ830Series

Connect with Toshiba on Twitter at twitter.com/ToshibaUSA, on Facebook at www.facebook.com/ToshibaUS, and on YouTube at www.youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of four business units: Digital Products Division, Imaging Systems Division, Storage Device Division, and Telecommunication Systems Division. Together, these divisions provide digital products, services and solutions, including industry-leading portable computers; televisions, TV/DVD Combination products, Blu-ray Disc and DVD products, and portable devices; imaging products for the security, medical and manufacturing markets; storage products for automotive, computer and consumer electronics applications; and IP business telephone systems with unified communications, collaboration and mobility applications. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation is a world leader and innovator in pioneering high technology, a diversified manufacturer and marketer of advanced electronic and electrical products spanning digital consumer products; electronic devices and components; power systems, including nuclear energy; industrial and social infrastructure systems; and home appliances. Toshiba was founded in 1875, and today operates a global network of more than 490 companies, with 203,000 employees worldwide and annual sales surpassing 6.3 trillion yen (US$77 billion). Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

© 2011 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved. Ultrabook is a trademark of Intel Corporation in the U.S. and/or other countries.

1 Weight. Weight may vary. See Weight Legal Footnote at www.info.toshiba.com

2 Price. Reseller prices may vary. MSRP means “Manufacturer’s Suggested Retail Price.”

3 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com

4 Solid State Drive Capacity. Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Solid State Drive Capacity Legal Footnote at www.info.toshiba.com

5 The “USB Sleep & Charge function” may not work with certain external devices even if they are compliant with the USB specification. In those cases, turn the power of the computer ON to charge the device.

Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=6847899&lang=en

Access Communications
Jared Leavitt, 415-867-5328
jared@accesspr.com

Multimedia Files:

The sub-2.5 pound Toshiba Portege Z830 Ultrabook, the world's lightest 13-inch platform. (Photo: Business Wire) 2400 x 1819 jpg 433 KB
View all news