View all news

Introducing Toshiba USB 3.0 Flash Drives and Micro SD Memory Cards

09/25/2013

Toshiba’s commitment to storage grows with two new flash memory solutions

IRVINE, Calif.--(BUSINESS WIRE)--Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the Toshiba Micro Secure Digital (micro SD) class 10 UHS-I Memory cards and Toshiba TransMemory® USB 3.0 Flash Drive.

“Toshiba originally invented and have since perfected NAND flash memory technology, which both of these products utilize,” said Maciek Brzeski, vice president of product marketing and development of branded storage products, Toshiba America Information Systems, Inc., Digital Products Division. “Both of these removable storage solutions offer industry-proven quality and reliability with leading speeds, performance and capacities.”

Toshiba TransMemory™USB 3.0 Flash Drives

For consumers who need to drag and drop files quickly and safely between computing devices, Toshiba’s TransMemory USB 3.0 Flash Drives are an efficient ultraportable storage solution that offers high-speed data transfer and secure data protection.

This new line of flash drives provides consumers with a reliable and convenient way to store and transfer photos, videos, music and important digital files while on the go, as they work with any device equipped with USB port. These flash drives not only make it easy to transfer files, but more importantly, they protect consumers’ data against theft and loss. The downloadable password protection security software that comes included with the drives allows users to create public and private partitions to ensure that their critical data is always protected.

Toshiba’s TransMemory USB 3.0 Flash Drives are optimized for devices with a USB 3.0 port for high-speed data transfer of up to 70 MB/s31, but are also backward compatible and work with devices that are only equipped with a USB 2.0 port. Additionally, these flash drives are plug and play-enabled for easy installation and are compatible with both Windows and Mac operating systems. They are available in 16GB, 32GB and 64GB capacities2 and all come with a five-year limited warranty.

Toshiba Micro Secure Digital Class 10 UHS-I Memory Cards

Toshiba’s microSD Class 10 UHS-1 memory card provides consumers who are looking to extend the storage capacity of their mobile devices, including smartphones and tablets, with a simple removable solution. These memory cards offer high-speed performance and reliability, and are backed by a 5-year limited warranty. A full-sized SD adapter is also included to ensure the memory cards’ compatibility with all standard SD devices, such as digital cameras, camcorders and laptops. With transfer speeds of up to 30 MB/s3, users will enjoy speedy data transfer times between PCs and mobile devices. The Toshiba microSD Class 10 UHS-1 memory cards are available in a number of different capacities, including 8GB, 16GB, 32GB and 64GB.4

Pricing and Availability

The Toshiba TransMemory USB 3.0 Flash Drives will be available for purchase at select retailers and on ToshibaDirect.com in October 2013. The 16GB flash drive will be $29.99 MSRP, the 32GB flash drive will be $49.99 MSRP and the 64GB flash drive will be $99.99 MSRP.

The Toshiba Micro Secure Digital Class 10 UHS-I Memory Cards will be available for purchase at select retailers and on ToshibaDirect.com in October 2013. The 8GB memory card will be $19.99 MSRP, the 16GB memory card will be $39.99 MSRP, the 32GB memory card will be $69.99 MSRP and the 64GB memory card will be $99.99 MSRP.

Image Gallery http://bit.ly/1aOVeKt

Connect with Toshiba on Facebook at www.facebook.com/ToshibaUSA, on Twitter at twitter.com/ToshibaUSA, and on YouTube at youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of three business units: Digital Products Division, Imaging Systems Division, and Telecommunication Systems Division. Together, these divisions provide digital products, services and solutions, including industry-leading portable computers; televisions, TV/DVD Combination products, Blu-ray Disc™ and DVD products, and portable devices; imaging products for the security, medical and manufacturing markets; storage products for computers; and IP business telephone systems with unified communications, collaboration and mobility applications. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation is a world leader and innovator in pioneering high technology, a diversified manufacturer and marketer of advanced electronic and electrical products spanning digital consumer products; electronic devices and components; power systems, including nuclear energy; industrial and social infrastructure systems; and home appliances. Toshiba was founded in 1875, and today operates a global network of more than 490 companies, with 203,000 employees worldwide and annual sales surpassing 6.3 trillion yen (US$77 billion). Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

© 2013 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

1 Maximum read speed 70 MB/s, write speed lower. Based on Toshiba internal test results, read and write speeds may vary depending on user-specifications such as devices used and files size read or written

2 Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10.

3 Maximum read speed 30 MB/s; write speed lower. Based on Toshiba internal test results, read and write speeds may vary depending on user-specifications such as devices used and files size read or written.

4 Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10.

Toshiba
Eric Paulsen, 949-583-3541
eric.paulsen@tais.toshiba.com
or
Access Communications
Jared Ricardo, 415-844-6232
jricardo@accesspr.com

Multimedia Files:

View all news