Powerful SRLED's Provide Illumination Angle Of 53 Degrees, Eliminates Need For Additional Cameras And Lighting
Toshiba Surveillance & IP Video Products Group, a business unit of
Toshiba America Information Systems, Inc., today introduced its new,
advanced IK-WB81A IP bullet camera with full 1080p HD resolution.
Designed for outdoor video surveillance, the IK-WB81A captures a wider
field of view than competitive bullet cameras by using an exclusive,
long-range SRLED (Single Reflex LED) IR system with an illumination
angle of 53 degrees.
"Our new IK-WB81A offers a 30 meter viewing range which takes advantage
of the 1080p HD resolution," said Sergio Collazo, Director - Sales &
Marketing, Toshiba Surveillance & IP Video Products Group. "That means
you can discreetly monitor larger outdoor areas at night without
incurring the cost of additional hardware."
No More "Halo" Effect
The IK-WB81A is ideal for video surveillance applications that
experience changing light conditions throughout the day and require
extra illumination at night. Its Vari-focal 3.7mm to 9mm zoom lens and
SRLED IR illuminators are complimented by new Split Glass technology
that prevents LED light from reflecting back into the lens. Split Glass
eliminates the washed-out "halo" effect often seen on nighttime images,
especially when the lens glass is dirty or wet. Also, the IK-WB81A
features day/night imaging with IR cut filter and wide dynamic range for
difficult backlighting conditions.
Fast, Simple Installation
The IK-WB81A installs quickly and easily. It comes standard with
simplified cable management, remote optical zoom and one-touch remote
auto focus to eliminate the need for contractors to run back and forth
to the control room to confirm proper focus. ONVIF compliance makes the
IK-WB81A interoperable with third-party ONVIF components, regardless of
the manufacturer.
Additional features of the IK-WB81A include:
-
Wide viewing angle: 37° to 96° horizontal, 21° to 53° vertical
-
Choice of H.264, MPEG4 and MJPEG compression codecs
-
Up to 30 fps at full HD 1920 x 1080 resolution
-
HD image quality to capture facial features, license plates and the
smallest of details
-
IP66 weatherproof protection rating to withstand outdoor elements
-
Audio in/out
-
SD card slot for edge recording.
For more information, visit www.toshibasecurity.com.
Or call 1-877-855-1349.
ABOUT TOSHIBA AMERICA INFORMATION SYSTEMS, INC.
Headquartered in Irvine, Calif., TAIS is comprised of three business
units: Digital Products Division, Imaging Systems Division, and
Telecommunication Systems Division. Together, these divisions provide
digital products, services and solutions, including industry-leading
portable computers; televisions, TV/DVD Combination products, Blu-ray
Disc™ and DVD products, and portable devices; imaging products for the
security, medical and manufacturing markets; storage products for
computers; and IP business telephone systems with unified
communications, collaboration and mobility applications. TAIS provides
sales, marketing and services for its wide range of products in the
United States and Latin America. TAIS is an independent operating
company owned by Toshiba America, Inc., a subsidiary of Toshiba
Corporation. For more information on TAIS visit us.toshiba.com.
ABOUT TOSHIBA CORPORATION
Toshiba Corporation is a world leader and innovator in pioneering high
technology, a diversified manufacturer and marketer of advanced
electronic and electrical products spanning digital consumer products;
electronic devices and components; power systems, including nuclear
energy; industrial and social infrastructure systems; and home
appliances. Toshiba was founded in 1875, and today operates a global
network of more than 490 companies, with 203,000 employees worldwide and
annual sales surpassing 6.3 trillion yen (US$77 billion). Visit
Toshiba's web site at www.toshiba.co.jp/index.htm.
©2013 Toshiba America Information Systems, Inc. All product names and
trademarks belong to their respective owners. Information in press
releases, including without limitation product prices, specifications,
and contact information, is current on date of the release, and is
subject to change without notice. Reseller prices may vary.