Industry-First 4K Chipset Converts HDMI® Signal to MIPI® dual-DSI Interface on Small Form-Factor Ultra HD LCD Displays
Toshiba
America Electronic Components, Inc. (TAEC)*, a committed leader that
collaborates with technology companies to create breakthrough designs,
today adds the TC358870XBG Display Serial Interface (DSI) to its family
of mobile peripheral IC products.
The TC358870XBG is a 4K High Definition Multimedia Interface (HDMI®)
to MIPI® dual-DSI converter chipset with video format
conversion. This is the first and only device in the market that enables
direct 4K HDMI video input to LCD displays with MIPI dual-DSI interface,
allowing small, form factor high-resolution mobile displays to be used
in consumer and industrial applications.1
"The TC358870XBG provides design, performance and cost benefits making
it suited for small, mobile consumer electronics and industrial products
with high-resolution LCD displays requiring MIPI dual-DSI input," says
Deepak Prakash, senior director for the Logic LSI Business Unit, System
LSI Group at TAEC. "Application Processors with an HDMI interface used
in traditional larger displays can now drive up to 3840 x 2160 display
resolution in next-generation small form factor mobile devices including
head-mounted displays (HMDs), digital camera displays, hand- held gaming
accessories and wearable computing devices."
The TC358870XBG's 297 MHz HDMI input supports up to 3840 x 2160 @ 24bpp
at a refresh rate of 30 fps and 2560 x 1600 @ 24bpp at a refresh rate of
60 fps. The device supports common 3D video formats and protocols
compatible with the HDMI 1.4 standard. The TC358870XBG supports a MIPI
dual DSI interface up to 8Gbps.
The Toshiba TC358870XBG is an 80-pin device for non-HDI boards with a
small package size of 7.0 x 7.0 mm, 0.65 mm ball pitch and 1.2 mm
maximum height.
Pricing and Availability
Sample pricing for the TC358870XBG device is $5.00 (U.S.). Sample
shipments are currently available with mass production scheduled for
September, 2014.
*About TAEC
Through proven commitment, lasting relationships and advanced, reliable
electronic components, Toshiba enables its customers to create
market-leading designs. Toshiba is the heartbeat within product
breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip
companies worldwide. A committed electronic components leader, Toshiba
designs and manufactures high-quality flash memory-based storage
solutions, solid state drives (SSDs), hard disk drives (HDDs), solid
state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs,
imaging products, microcontrollers, wireless components, mobile
peripheral devices, advanced materials and medical tubes that make
possible today’s leading smartphones, tablets, cameras, medical devices,
automotive electronics, industrial applications, enterprise solutions
and more.
Toshiba
America Electronic Components, Inc. is an independent operating
company owned by Toshiba America, Inc., a subsidiary of Toshiba
Corporation, Japan’s largest semiconductor manufacturer and the world’s
sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide
Semiconductor Revenue, December 2013). Toshiba Corporation was founded
in 1875 and today has over 554 subsidiaries and affiliates, with 206,087
employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
1Source: Toshiba America Electronic Components,
Inc., research as of 4/11/2014. here.
HDMI is a registered trademark of HDMI Licensing, LLC in the United
States and/or other countries.
MIPI is a registered trademark of MIPI Alliance, Inc.
Information in this press release, including product pricing and
specifications, content of services and contact information, is current
and believed to be accurate on the date of the announcement, but is
subject to change without prior notice. Technical and application
information contained here is subject to the most recent applicable
Toshiba product specifications. In developing designs, please ensure
that Toshiba products are used within specified operating ranges as set
forth in the most recent Toshiba product specifications and the
information set forth in Toshiba’s "Handling Guide for Semiconductor
Devices," or "Toshiba Semiconductor Reliability Handbook." This
information is available athttp://www.toshiba.com/taec/support/techquestions/index.jsp,
or from your TAEC representative.
APIC 14 710