View all news

Newest Toshiba 2-Channel Brushed DC Motor Driver IC Supports High Voltages and Currents Required by Industrial and Office Automation Equipment under Continuous Operation

08/26/2013

Range of Package Sizes and Reliability Features Make Device Ideal Choice for a Wide Variety of Applications

Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced the newest addition to the company's motor driver family, the TB67H400A. The new device is a 2-channel motor driver IC supporting the high voltage and current requirements of brushed DC motors in industrial and office automation (OA) equipment under continuous operation. Package and reliability features of the TB67H400A improve operation for a variety of applications such as home appliances, ATMs, banknote recognition equipment, amusement park machines and office automation equipment.

"Continuous operation requires industrial and OA equipment that have reliable thermal management or there will be system failure," says Andrew Burt, vice president of the Analog and Imaging Business Unit, System LSI Group at TAEC. "In addition, these systems need to be quiet, low energy and as efficient as possible . Toshiba is creating a large portfolio of motor control drivers that satisfy these requirements for many different classes of motors in industrial and OA equipment ."

TAEC leveraged its latest high-voltage analog process in the design of the TB67H400A. The device realizes a 50V maximum rating and low-on resistance of 0.5 Ω (maximum, sum of the upper and lower side MOSFETs) during motor drive output, thereby creating a maximum operating current of 3.0 A(4.0A rated), per channel, for a 2-channel drive. Toshiba's unique parallel channel control function (high-current mode) delivers a 6 .0A maximum operating current (8.0A rated) when 2-channel outputs are used as a 1-channel driver.

The driver IC is available in a four package line-up to address various customer requirements. A thermally efficient ZIP package improves power dissipation for applications that need a continuous motor drive at high current. Small QFN and HTSSOP packages enable downsizing of equipment and reduction of material costs. An HSOP package allows flow soldering on a paper phenolic board which helps reduce cost of printed circuit board development.

The TB67H400A integrates abnormality detection functions for high reliability. The IC includes a thermal shutdown circuit, over-current shutdown circuit, and under-voltage lockout circuit.

Pricing and Availability

Sample pricing for the TB67H400A is $ 2.40 (U.S.). Sample shipments begin today with mass production scheduled for October, 2013.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's fifth largest semiconductor manufacturer (Gartner, 2012 Worldwide Semiconductor Revenue, April, 2013). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba's "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook." This information is available at http://www.toshiba.com/taec/support/techquestions/index.jsp or from your TAEC representative.

APIC 13 686

Multimedia Files:

View all news