Adds 32GB product and "Internet Pass thru Mode" feature to make wireless connection to the Internet more convenient
Toshiba Corporation (TOKYO:6502) today announced the expansion of its
line-up of "FlashAir™", the SDHC memory card with embedded wireless LAN
communications, with the launch of the latest 32GB card. The new card
will go on sale on November 16th in the Japanese market, and sales in
markets around the world will follow.
"FlashAir™" is an SDHC memory card that incorporates a wireless LAN chip
set plus an antenna for wireless communications. The card supports
wireless sharing and transfers of photos from digital cameras to
smartphones and tablets.
The new 32GB card has a new feature, "Internet pass thru mode", which
enables Internet connection even while the smartphone is connected to
FlashAir™, by using other access points, such as the wireless LAN router
in the home. With the new feature, users do not have to manually change
the wireless network settings of smartphones when downloading photos
from the card to smartphones, uploading photos to SNS from a smartphone,
or sending email.[1] The new feature can also be used in the
current FlashAir™ W-02 line-up (product names: "SD-WC008G" and
"SD-WC016G") by updating the firmware of the card.[2]
Toshiba will reinforce and extend its leadership of the memory business
by further enhancing its FlashAir™ line-up.
Outline of the New Product
|
Product Name
|
|
Capacity
|
|
Speed Class
|
|
Price
|
|
Start of Sales
|
|
SD-WD032G
|
|
32GB[3]
|
|
Class 10
|
|
Open
|
|
Nov. 16th, 2013 in Japan
|
Current Line-up in Japan
|
Product Name
|
|
Capacity
|
|
Speed Class
|
|
SD-WC008G
|
|
8GB
|
|
Class 10
|
|
SD-WC016G
|
|
16GB
|
|
Class 10
|
Main Specifications of the New Product
|
Series Name
|
|
FlashAir™ W-02
|
|
Product Name
|
|
SD-WD032G
|
|
Capacity
|
|
32GB
|
|
Speed Class
|
|
Class 10
|
|
Compliant Standard
|
|
SD Memory Card Standard Ver.4.00
|
|
Wireless LAN Standard
|
|
IEEE802.11 b/g/n
|
|
Wireless LAN Security
|
|
WEP, TKIP, AES(WPA, WPA2)
|
|
Power Supply Voltage
|
|
2.7-3.6V
|
|
Operating Environment
|
|
Temperature: -25°C to 85°C Relative humidity: 95% at 25°C (no
condensation)
|
|
External Dimensions
|
|
32.0mm(L)×24.0mm(W)×2.1mm(T)
|
|
Weight
|
|
Approx.2g
|
Wireless LAN Supporting Regions
|
|
Please check the latest status on the following URL. URL:
http://www.toshiba.co.jp/p-media/wwsite/flashair.htm
|
Notes:
-
[1] It is necessary to set up the name of the access point (SSID) and
the password in advance to use "Internet pass thru mode". If you need
to connect to a different SSID, it is necessary to set up the name of
the access point and the password once again.
-
[2] The FlashAir™ firmware update download will be available from
November 18th at the following website.
http://www.toshiba.co.jp/p-media/english/download/wl/updatetool_w02.htm
"Internet
pass thru mode" is not available for FlashAir™ Class 6 products
(product names: "SD-WL008G" and "SD-WB008G").
-
[3] The product is labeled based on the memory chip(s) it contains,
not the amount of memory capacity available for data storage by the
end user. Part of the capacity is reserved for card functionality.
Minimum consumer-usable memory capacity is approximately 7.2GB for 8GB
products, approximately 14.4GB for 16GB products and approximately
28.8GB for 32GB products.
(For purposes of measuring memory
capacity in this context, 1 GB = 1,073,741,824 bytes.)
-
* Product names above are for the Japanese market.
-
* FlashAir™ is trademark of Toshiba Corporation.
Follow this link for more on "FlashAir™"
http://www.toshiba.co.jp/p-media/wwsite/flashair.htm
Information in this document, including product prices and
specifications, content of services and contact information, is current
on the date of the announcement but is subject to change without prior
notice.