Docking Station Transforms Laptop Into Comprehensive Desktop Experience Through Single Cable Connection Providing Faster Speed and Improved Graphics
Toshiba's
Digital Products Division (DPD), a division of Toshiba America
Information Systems, Inc., today announced a highly affordable new
addition to its line of award-winning universal docking stations, the
dynadock® V3.0. The dynadock V3.0 is the ideal one-cable connection that
instantly and effortlessly "docks" any Windows®-based laptop to an extra
monitor and multiple devices at any given time. Toshiba's new docking
station provides users with faster speed and improved graphics than its
predecessor due to the addition of USB 3.01 ports and HDMI
out support.
"The dynadock V3.0 really shines because its USB 3.0 connection creates
a workstation that any user can easily connect/disconnect and even share
with other users" said Phil Osako, Senior Director PC Marketing, Toshiba
America Information Systems, Inc., Digital Products Division. "This
versatile product makes using all of your devices simple and even helps
to clean up the user's desk space with its compact size."
Toshiba's small and sleek dynadock V3.0 hosts an HDMI out supporting
both video and 5.1 channel audio. In addition it has six powerful USB
ports, including two front USB 3.0 ports with Toshiba USB Sleep & Charge2
and four rear USB 2.0 ports to significantly boost sharing and
productivity, creating a full-service workstation wherever a user
chooses to set it up. Like Toshiba's dynadock U3.0, it also serves as a
convenient hub that connects the users' main laptop or desktop to all of
their peripheral gadgets via one cable, eliminating unnecessary clutter
on their desk. It is compatible with a large-screen HD display, variety
of USB powered gadgets, including full-size keyboard and mouse, external
storage, printer, optical drive, and more.
The unit's USB 3.0 connection and built-in HD graphics cards support up
to 2048x1152 resolution, delivering faster frame rates and
higher-resolution image than would normally be seen on a PC. This
elevates the movie watching, gaming and media streaming to a richer
level. Whether users are turning to their laptop for work or play, the
dynadock V3.0 has the ability to transform their computing system into a
comfortable and convenient desktop experience.
Pricing and Availability
Toshiba's dynadock V3.0 is currently available for purchase at major
retailers, e-tailers and direct from Toshiba at ToshibaDirect.com,
for a starting price of $119.99 MSRP3.
Image Gallery: http://bit.ly/toshibadynadockv.
Connect with Toshiba on Facebook at www.facebook.com/ToshibaUSA,
on Twitter at twitter.com/ToshibaUSA,
and on YouTube at youtube.com/ToshibaUS.
About Toshiba America Information Systems, Inc. (TAIS)
Headquartered in Irvine, Calif., TAIS is comprised of three business
units: Digital Products Division, Imaging Systems Division, and
Telecommunication Systems Division. Together, these divisions provide
digital products, services and solutions, including industry-leading
portable computers; televisions, TV/DVD Combination products, Blu-ray
Disc™ and DVD products, and portable devices; imaging products for the
security, medical and manufacturing markets; storage products for
computers; and IP business telephone systems with unified
communications, collaboration and mobility applications. TAIS provides
sales, marketing and services for its wide range of products in the
United States and Latin America. TAIS is an independent operating
company owned by Toshiba America, Inc., a subsidiary of Toshiba
Corporation. For more information on TAIS visit us.toshiba.com.
About Toshiba Corporation
Toshiba is a world-leading diversified manufacturer, solutions provider
and marketer of advanced electronic and electrical products and systems.
Toshiba Group brings innovation and imagination to a wide range of
businesses: digital products, including LCD TVs, notebook PCs, retail
solutions and MFPs; electronic devices, including semiconductors,
storage products and materials; industrial and social infrastructure
systems, including power generation systems, smart community solutions,
medical systems and escalators & elevators; and home appliances. Toshiba
was founded in 1875, and today operates a global network of more than
590 consolidated companies, with 206,000 employees worldwide and annual
sales surpassing 5.8 trillion yen (US$61 billion). Visit Toshiba's web
site at www.toshiba.co.jp/index.htm.
© 2013 Toshiba America Information Systems, Inc. All product, service
and company names are trademarks, registered trademarks or service marks
of their respective owners. Information including without limitation
product prices, specifications, availability, content of services, and
contact information is subject to change without notice. All rights
reserved.
1. USB
3.0. 5Gbps is the maximum theoretical interface transfer rate per
the specifications of the Universal Serial Bus 3.0. Actual transfer rate
will vary depending on your system configuration and other factors.
2. The "USB
Sleep & Charge function" may not work with certain external
devices even if they are compliant with the USB specification. In those
cases, turn the power of the computer ON to charge the device.
3. Price
as shown is after rebate, if any, applicable to that product and price
may also be subject to special offer requirements. Prices,
specifications, availability and terms of offer are subject to change
without notice. Toshiba is not liable for pricing, typographical or
photography errors. Reseller/Retailer pricing may vary.