View all news

Toshiba Announces Availability of Satellite Radius 12 Convertible Laptop

10/13/2015
  • 12.5-inch compact convertible Windows 10 PC equipped with expert screen, sound and performance technology from Technicolor, Corning, Harman Kardon, DTS and Intel
  • 4K Ultra HD display option, Durable Corning Gorilla Glass NBT and Windows Hello-capable
  • Available from Best Buy stores starting on October 18, 2015

Toshiba’s Digital Products Division (DPD), a division of Toshiba America Information Systems, Inc., today announced the availability of the Satellite Radius™ 12, the world’s first 12.5-inch convertible Windows 10 laptop with a 4K Ultra HD display. Available at Best Buy stores and BestBuy.com, the Satellite Radius 12 features top-of-the-line screen and sound quality, a sleek, lightweight design and a 6th generation Intel® Core™ processor1 that delivers maximum mobile performance and solid battery life.

“Our design goal was to develop a highly compact, versatile PC that does not compromise on performance or functionality to meet the needs of today’s discerning content creator,” said Philip Osako, senior director of product marketing, Toshiba America Information Systems, Inc., Digital Products Division. “Toshiba has created the ultimate companion for the highly mobile, digital consumer that requires versatility, portability and durability with top-of-the-line technology that enables them to fully take advantage of Windows 10 and enhance their productivity and creativity.”

Technicolor Certified 4K Display Enhanced by Corning Gorilla Glass NBT

The Satellite Radius 12 can be configured with a brilliant 12.5-inch diagonal touchscreen display with a native 4K Ultra HD (3840 x 2160) resolution that yields 352 pixels per inch, four times as many as a Full HD display. The display is calibrated and certified by the color experts Technicolor® and the device includes Chroma Tune™ for Toshiba software, which allows the user to select the best color scheme for the content they are using. Also available with a Full HD (1920 x 1080) IPS display option, both models feature a high-brightness 350-nit screen for use outdoors and IPS technology that provides wide viewing angles.

The laptop’s display is built with Corning® Gorilla® Glass NBT™, which offers 8x-10x higher scratch resistance than soda lime glass displays, plus reduced incidence of damage when inadvertently closing the display on top of an object and a better ability to withstand the shock of accidental bumps.

“Taking full advantage of touch notebook displays exposes the device to potential abuses that come with gripping, swiping, wiping and tapping. Today, a higher level of damage resistance is essential,” said John Bayne, vice president and general manager, Gorilla Glass, Corning Incorporated. “We developed Corning Gorilla Glass NBT to withstand the rigorous lifestyle of the latest generation convertible touchscreen PC’s and Toshiba’s Satellite Radius 12 is the perfect example.”

Small Laptop, Big Listening Experience

Continuing Toshiba’s tradition of offering high quality audio across its line of laptops, the Satellite Radius 12 includes a custom-designed adaptive audio system engineered by Harman Kardon® and Toshiba specifically for convertible laptops. Embedded sub-miniature speakers designed and tuned by the audio experts at Harman Kardon deliver sophisticated, rich audio that changes automatically depending on the laptop’s viewing mode so the sound quality and reach aligns with the screen viewing position. Audio processing software by DTS® further tunes the speakers for volume and quality.

“Convertible laptops offer a distinct challenge when trying to deliver great audio in multiple modes as the speaker placement is not stationary anymore,” said Michael Mauser, EVP and President of Lifestyle Division, HARMAN International. “Through our long-standing collaboration with Toshiba, we have designed an innovative adaptive audio solution that achieves optimized high-quality audio no matter what position the laptop is in so customers experience great sound from every angle.”

Facial Authentication with Windows Hello

The Satellite Radius 12 is one of the first PC’s to enable facial authentication with Windows Hello. Powered by an on-board infrared camera that provides a personal, convenient and password-free way to instantaneously log into the device and quickly get to work or play.

The Satellite Radius 12 also accelerates the new features and capabilities of Windows 10. For voice apps like Cortana and Skype, the Satellite Radius 12 features multi-directional TruTalk™ microphones, which offer clear voice detection, even in noisy environments and a dedicated Cortana key for easily calling up the personal digital assistant in Windows 10.

Maximum Mobile Performance, Maximum Connectivity

The laptops are powered by a 6th generation Intel Core processor, 8GB of RAM2 and can be configured with a 256GB or 512GB solid state drive3. In addition, the Satellite Radius 12 features ultra-fast 802.11ac Wi-Fi® and Bluetooth® plus a full range of ports including HDMI® capable of 4K output, one reversible USB Type-C connector that enables lightning fast data transfers over USB 3.1 and two Super Speed USB 3.0 ports. One USB 3.0 port features USB Sleep & Charge technology4, which can power mobile devices even when in sleep mode and delivers faster charging speeds when the laptop is off.

Designed for Travel

The Satellite Radius 12 features a sleek, highly-mobile compact design housed in durable aluminum to safeguard against the rigors of daily use. Designed for travel, the device weighs just 2.9 pounds5 with a slim 0.6-inch profile. The Satellite Radius 12 4K Ultra HD Edition features a Brushed Metal Finish in Carbon Gray, while the Full HD model features a Brushed Metal Finish in Silver. Both include LED backlit keyboards.

Pricing and Availability

The Satellite Radius 12 is available for purchase starting on October 18, 2015 from Best Buy, BestBuy.com and Microsoft Stores, as well as direct from Toshiba on toshiba.com/us for $1,299.99 MSRP6 for the 4K Ultra HD Edition and $999.99 MSRP for the Standard HD model.

Image Gallery: bit.ly/SatelliteRadius12

Connect with Toshiba on Facebook at www.facebook.com/ToshibaUSA, on Twitter at twitter.com/ToshibaUSA, and on YouTube at youtube.com/ToshibaUS.

About Toshiba America Information Systems, Inc. (TAIS)

Headquartered in Irvine, Calif., TAIS is comprised of five business units: Business Solutions Division, Digital Products Division, Imaging Systems Division, Telecommunication Systems Division and Industrial Solutions & Services Division. Together, these divisions provide digital products, services and solutions, including award-winning notebook computers, tablets, branded storage products, digital display solutions and cloud services; imaging products for the security, medical and manufacturing markets; IP business telephone systems with unified communications, collaboration and mobility applications; and IoT solution development, data analytics and IT services. TAIS provides sales, marketing and services for its wide range of products in the United States and Latin America. TAIS is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.

About Toshiba Corporation

Toshiba Corporation, a Fortune Global 500 company, channels world-class capabilities in advanced electronic and electrical product and systems into five strategic business domains: Energy & Infrastructure, Community Solutions, Healthcare Systems & Services, Electronic Devices & Components, and Lifestyles Products & Services. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future,” Toshiba promotes global operations and is contributing to the realization of a world where generations to come can live better lives. Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global network of over 580 consolidated companies employing 199,000 people worldwide, with annual sales surpassing 6.6 trillion yen (US$55 billion). To find out more about Toshiba, visit www.toshiba.co.jp/index.htm

© 2015 Toshiba America Information Systems, Inc. All product, service and company names are trademarks, registered trademarks or service marks of their respective owners. Information including without limitation product prices, specifications, availability, content of services, and contact information is subject to change without notice. All rights reserved.

1 Processor. CPU performance may vary. See Processor Legal Footnote at www.info.toshiba.com

2 Memory. Memory size may vary. See Memory Legal Footnote at www.info.toshiba.com

3 Solid State Drive Capacity. Drive capacity may vary. One Gigabyte (GB) means 109 = 1,000,000,000 bytes using powers of 10. See Solid State Drive Capacity Legal Footnote at www.info.toshiba.com

4 The “USB Sleep & Charge function” may not work with certain external devices even if they are compliant with the USB specification. In those cases, turn the power of the computer ON to charge the device.

5 Weight may vary. See Weight Legal Footnote at www.info.toshiba.com

6 Reseller prices may vary. MSRP means “Manufacturer's Suggested Retail Price.”

Access Communications
Yulimar Chiu, 415-844-6240
ychiu@accesspr.com

Multimedia Files:

View all news