Provide Military Grade Protection For Sensitive Data with Innovative Hardware Security Device, Up to 32 GB
Toshiba’s Digital
Products Division (DPD), a division of Toshiba America Information
Systems, Inc., today introduced the Toshiba Encrypted USB Flash Drive, a
device that utilizes a hardware based encryption process to deliver a
robust, secure (military grade AES 256-bit encryption)1, easy
to use and affordable solution to safely make sensitive data portable.
Ideal for enterprise companies, government agencies and concerned
consumers, the Toshiba Encrypted USB Flash Drive offers a higher
assurance of security.
Available in 4GB, 8GB, 16GB and 32GB2 capacities, the Toshiba
Encrypted USB Flash Drive uses a built-in mini-keyboard to authenticate
access, incorporating a rechargeable battery so the user can enter a
secure code before plugging into a USB port. Users simply enter their
secure PIN and plug the drive into any USB 2.0 port on a compatible
device. Once access is granted, the drive “unlocks” the media,
permitting clearance to all of the content stored on the drive. When the
drive is removed from a USB port, the drive automatically re-locks and
encrypts the stored media.
“There is a heightened sense of awareness that confidential content is
at risk,” said Maciek Brzeski, Vice President of Branded Storage
Products, Toshiba Digital Products Division. “Toshiba developed the
Encrypted USB Flash Drive as a new way to provide portable data security
with one of the highest encryption standards available on the market.”
Should the Toshiba Encrypted USB Flash Drive become lost or stolen, it
is equipped with a Brute Force Hack Defense Mechanism that will render
all stored information irrecoverable after 10 consecutive unsuccessful
attempts to enter the secure PIN. The Toshiba Encrypted USB Flash Drive
also carries a FIPS (Federal Information Processing Standards)
Publication 140-2 Level 3 certification, issued by the National
Institute of Standards and Technology (NIST), a certification often
required by government agencies and other data security sensitive
industries, such as healthcare and finance. The Toshiba Encrypted USB
Flash Drive incorporates DataLock® Technology by ClevX, LLC.
Pricing and Availability2,4
Beginning today, the Encrypted USB Flash Drive is available for purchase
at select retailers and on toshiba.com/us/flash-drives
for $95.00 MSRP for the 4GB model, $112.00 MSRP for the 8GB model,
$140.00 MSRP for the 16GB and $200.00 MSRP for the 32GB model. A 3 Year
Standard Limited Warranty3 is included with all models.
Image Gallery: http://bit.ly/ToshibaEncryptedUSB
Connect with Toshiba on Facebook at facebook.com/ToshibaUSA,
on Twitter at twitter.com/ToshibaUSA
and on YouTube at youtube.com/ToshibaUS.
About Toshiba America Information Systems, Inc. (TAIS)
Headquartered in Irvine, Calif., TAIS is comprised of four business
units: Business Solutions Division, Digital Products Division, Imaging
Systems Division, and Telecommunication Systems Division. Together,
these divisions provide digital products, services and solutions,
including industry-leading notebook computers, tablets and All-in-One
computers, televisions, TV/DVD Combination products, Blu-ray Disc™, DVD
players and media boxes, as well as cloud services; imaging products for
the security, medical and manufacturing markets; storage products for
computers; and IP business telephone systems with unified
communications, collaboration and mobility applications. TAIS provides
sales, marketing and services for its wide range of products in the
United States and Latin America. TAIS is an independent operating
company owned by Toshiba America, Inc., a subsidiary of Toshiba
Corporation. For more information on TAIS visit us.toshiba.com.
About Toshiba
Toshiba Corporation, a Fortune Global 500 company, channels world-class
capabilities in advanced electronic and electrical product and systems
into five strategic business domains: Energy & Infrastructure, Community
Solutions, Healthcare Systems & Services, Electronic Devices &
Components, and Lifestyles Products & Services. Guided by the principles
of The Basic Commitment of the Toshiba Group, “Committed to People,
Committed to the Future”, Toshiba promotes global operations towards
securing “Growth Through Creativity and Innovation”, and is contributing
to the achievement of a world in which people everywhere live in safe,
secure and comfortable society.
Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global
network of over 590 consolidated companies employing over 200,000 people
worldwide, with annual sales surpassing 6.5 trillion yen (US$63
billion). To find out more about Toshiba, visit www.toshiba.co.jp/index.htm
© 2015 Toshiba America Information Systems, Inc. All rights reserved.
DataLock is a trademark or registered trademark of ClevX, LLC. Blu-ray
Disk is a trademark of the Blu-Ray Disc Association. All other products
and names are the property of their respective owners. Information
including without limitation product prices, specifications,
availability, content of services, and contact information is subject to
change without notice.
1 Advanced Encryption Standard (AES) is a specification for
the encryption of electronic data established by the U.S. National
Institute of Standards and Technology (NIST).
2 One Gigabyte (1GB) means 109 = 1,000,000,000
bytes and One Terabyte (1TB) means 1012 = 1,000,000,000,000
bytes using powers of 10. A computer operating system, however, reports
storage capacity using powers of 2 for the definition of 1GB= 230
= 1,073,741,824 bytes and 1TB = 240 = 1,099,511,627,776
bytes, and therefore shows less storage capacity. Available storage
capacity (including examples of various media files) will vary based on
file size, formatting, settings, software, operating system and other
factors.
3 The terms and conditions of Toshiba’s standard limited
warranty are available at www.warranty.toshiba.com.
4 Reseller prices may vary. MSRP means “Manufacturer’s
Suggested Retail Price.”