New Line Includes First 2-in-1 Convertible PC to Offer 4K Ultra HD Screen Resolution, Making it Ideal Choice for Mobile Video and Photo Enthusiasts
Toshiba’s
Digital Products Division (DPD), a division of Toshiba America
Information Systems, Inc., today announced three new 2-in-1 convertible
PC designs: the 14-inch Satellite Radius™ 14, 15.6-inch Satellite Radius
15 and 15.6-inch Satellite Radius 15 4K Ultra HD Edition. Built for
Windows 10, these convertible PCs feature a precision 2-axis hinge,
allowing the screen to rotate a full 360-degrees, which converts the
devices from laptop to tablet and everything in between.
“A tremendous amount of R&D has gone into convertible PC design over
Toshiba’s 30-year history as a laptop leader,” said Philip Osako, senior
director of product marketing, Toshiba America Information Systems,
Inc., Digital Products Division. “Today, convertibility is all about
convenience – consumers can ditch multiple devices and get it all done
with one. We believe that by offering new thin and light designs, screen
options in resolutions from HD to 4K and a range of new, affordable
price points, we’re playing our part in further fueling the growth
potential of this category.”
Get It All Done With One™
Satellite Radius devices deliver the best of both worlds – the full
performance of a laptop plus the convenience of a tablet. A two-axis
flip-and-fold hinge enables a smooth transition into five different
viewing modes – Laptop, Tablet, Tabletop, Presentation and Audience. Get
work done on a slim, high-performance laptop then flip the screen to
conduct presentations, be entertained or browse comfortably in tablet
mode.
Brilliant 4K Display, Brilliant Audio
Toshiba was the first manufacturer to offer a consumer laptop with a 4K
Ultra HD display, and now is the first to deliver that brilliance in
a convertible laptop with the Satellite Radius 15 4K Ultra HD Edition.
With a stunning 3840 x 2160 resolution with 282 PPI (pixels per inch),
customers can enjoy movies, TV and photos in crystal-clear definition.
Built-in Harman Kardon® stereo speakers and DTS Sound™ plus exclusive
Slipstream™ port technology in the speakers that reduces distortion,
creates a more precise, rich sound at max volume for listening to your
favorite music or watching video while at work or home or on the go.
Built With Windows 10 in Mind
Designed to take advantage of the new experiences enabled by Windows 10
with smart performance and customized features built around the way you
work and play, these devices are also equipped with HD webcams and
TruTalk™ dual-array microphones to enable voice apps like Cortana and
Skype, plus a dedicated Cortana key for easy access to Microsoft’s
personal digital assistant.
These new 2-in-1 convertible PCs are thin and lightweight, featuring
sculpted lines and illuminated keyboards. The Satellite Radius 15
features a brushed-metal enclosure, while the Satellite Radius 14
features an all-new brushed resin black matte cover and a brushed-metal
palm rest. Powering Toshiba’s sleek new Satellite Radius 15 are 5th
generation Intel® Core™ processors1, enabling excellent
performance and multitasking. The Satellite Radius 14 is configurable
with a 5th generation Intel Core processor or an AMD Accelerated
Processing Unit (APU). To ensure that consumers are as productive as
possible, these devices are also available with 802.11ac Wi-Fi® and a
range of ports and extensions, including one USB 2.0 port, an SD card
slot and two Super Speed USB 3.0 ports2 that enable ultrafast
data transfers from external hard drives – one of which is equipped with
USB Sleep & Charge technology3 to enable the charging of
additional USB-powered devices even when the PC is powered off.
Pricing and Availability
The new Satellite Radius 14 and Satellite Radius 15 will be available
for purchase on June 21, 2015 at Best Buy and BestBuy.com, starting at
$584.99 MSRP4 for the Satellite Radius 14 and $842.99 MSRP
for the Satellite Radius 15.
The Satellite Radius 14 and 15 2-in-1 PCs will ship with Windows 8.1
pre-installed and are eligible for a free upgrade to Windows 10 when it
becomes available on July 295 at windows.com/Windows10upgrade.
Image Gallery
www.toshibapresscenter.com
Connect with Toshiba on Facebook at www.facebook.com/ToshibaUSA,
on Twitter at twitter.com/ToshibaUSA,
and on YouTube at youtube.com/ToshibaUS
About Toshiba America Information Systems, Inc. (TAIS)
Headquartered in Irvine, Calif., TAIS is comprised of four business
units: Business Solutions Division, Digital Products Division, Imaging
Systems Division, and Telecommunication Systems Division. Together,
these divisions provide digital products, services and solutions,
including award-winning notebook computers, tablets and All-in-One
computers, cloud services; imaging products for the security, medical
and manufacturing markets; storage products for computers; and IP
business telephone systems with unified communications, collaboration
and mobility applications. TAIS provides sales, marketing and services
for its wide range of products in the United States and Latin America.
TAIS is an independent operating company owned by Toshiba America, Inc.,
a subsidiary of Toshiba Corporation. For more information on TAIS visit us.toshiba.com.
About Toshiba Corporation
Toshiba Corporation, a Fortune 500 company, channels world-class
capabilities in advanced electronic and electrical product and systems
into five strategic business domains: Energy & Infrastructure, Community
Solutions, Healthcare Systems & Services, Electronic Devices &
Components, and Lifestyles Products & Services. Guided by the principles
of The Basic Commitment of the Toshiba Group, "Committed to People,
Committed to the Future", Toshiba promotes global operations towards
securing "Growth Through Creativity and Innovation", and is contributing
to the achievement of a world in which people everywhere live in safe,
secure and comfortable society. Founded in Tokyo in 1875, today's
Toshiba is at the heart of a global network of over 590 consolidated
companies employing over 200,000 people worldwide, with annual sales
surpassing 6.5 trillion yen (US$63 billion). To find out more about
Toshiba, visit www.toshiba.co.jp/index.htm
© 2015 Toshiba America Information Systems, Inc. All product, service
and company names are trademarks, registered trademarks or service marks
of their respective owners. Information including without limitation
product prices, specifications, availability, content of services, and
contact information is subject to change without notice. All rights
reserved.
1 Processor. CPU performance may vary. See Processor Legal
Footnote at www.info.toshiba.com
2 USB 3.0. 5Gbps is the maximum theoretical interface
transfer rate per the specifications of the Universal Serial Bus 3.0.
Actual transfer rate will vary depending on your system configuration
and other factors.
3 The “USB Sleep & Charge function” may not work with certain
external devices even if they are compliant with the USB specification.
In those cases, turn the power of the computer ON to charge the device.
4 Price. Reseller prices may vary. MSRP means “Manufacturer’s
Suggested Retail Price.”
5 Windows 10 Upgrade Offer valid for qualified Windows® 7 and
Windows 8.1 devices (including devices you already own) for one year
after Windows 10 upgrade availability. Visit
windows.com/windows10upgrade for more details.