New MG06 Series delivers 25 percent capacity increase over prior generation models
Toshiba
America Electronic Components, Inc. (TAEC), a committed technology
leader, today announces the 10TB
1
MG06 Series
Enterprise Capacity HDD model line-up. Toshiba’s new MG06 series offers
a 25 percent capacity increase compared to prior generations and enables
models to be delivered at multiple capacity points to better leverage
capacity refresh qualification cycles for OEMs/ODMs infrastructure
builders, cloud solution providers (CSPs) and system integrators.
In addition to a heftier capacity, the 10TB MG06 Series features a
greater maximum sustained transfer rate, 237 MiB/s2, than the
earlier MG05 Series, as well as a 25 percent increase in MTTF3,
with a rating of 2.5M hours. The drive provides a SATA 6Gbit/s interface4
and 7,200 rpm performance. Additionally, the MG06 HDD supports emulated
512 Advanced Format (512e) technology for compatibility with legacy
applications and operating environments; or 4K native sector technology
for optimum performance in all-disk or hybrid storage platforms.
“The volume and value of digital data across organizations of all sizes
continues to create opportunities and challenges for CSPs, server and
storage vendors, and IT professionals,” said Scott Wright, Director of
HDD Product Marketing at Toshiba America Electronic Components, Inc.
“Toshiba’s new MG06 Series advances performance and value across a range
of Enterprise Capacity HDD models to better align with the diverse needs
of systems and solutions for Cloud and Business Critical applications
today.”
Designed to support higher storage density, the MG06 Series HDD
introduces 10TB to Toshiba’s line-up while also updating 6TB and 8TB
capacities. Based on Toshiba’s latest HDD architecture, the new models
can save rack space to improve the operational efficiency of cloud-scale
infrastructure. The MG06 Series is engineered for mid-line, nearline,
and tier two business critical server and storage system workloads;
including servers supporting application workloads that benefit from
high capacity per spindle; capacity-optimized data center storage
systems; and enterprise IT and data center servers supporting workloads
per HDD of up to 550TB total bytes written and read per year. All models
feature Toshiba’s Persistent Write Cache Technology for peak performance
and enterprise-grade data reliability. Models also support power mode
management capabilities that conform to HDD industry standards.
Sample shipments of the MG06 SATA HDD model are now available. For more
information on Toshiba’s line of storage product, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html.
To learn more about Toshiba’s storage solutions visit the storage blog
at http://storage.toshiba.com/corporateblog/ and
follow @ToshibaStorage
on Twitter.
About Toshiba Corp. and Toshiba America Electronic Components, Inc.
(TAEC)
Through proven commitment, lasting relationships and advanced, reliable
electronic components, Toshiba enables its customers to create
market-leading designs. Toshiba is the heartbeat within product
breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip
companies worldwide. A committed electronic components leader, Toshiba
designs and manufactures high-quality flash memory-based storage
solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete
devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless
components, mobile peripheral devices, advanced materials and medical
tubes that make possible today’s leading smartphones, tablets, cameras,
medical devices, automotive electronics, industrial applications,
enterprise solutions and more.
Toshiba
America Electronic Components, Inc. is an independent operating
company owned by Toshiba America, Inc. For over 140 years, Toshiba
Corporation has contributed to a sustainable future by applying
innovative technologies to value creation. Today, our business domains
are centered on the essential infrastructure that supports modern life
and society. Guided by the principles of The Basic Commitment of the
Toshiba Group, “Committed to People, Committed to the Future”, Toshiba
promotes global operations that contribute to realization of a world
where generations to come can live better lives. Visit Toshiba's web
site at http://toshiba.semicon-storage.com.
© 2017 Toshiba America Electronic Components, Inc. All rights reserved.
Information in this press release, including product pricing and
specifications, content of services and contact information, is current
and believed to be accurate on the date of the announcement, but is
subject to change without prior notice. Technical and application
information contained here is subject to the most recent applicable
Toshiba product specifications.
1 Definition of capacity: Toshiba defines a megabyte (MB) as
1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte
(TB) as 1,000,000,000,000 bytes. A computer operating system, however,
reports storage capacity using powers of 2 for the definition of 1TB = 230
bytes = 1,099,511,627,776 bytes and therefore shows less storage
capacity. Available storage capacity (including examples of various
media files) will vary based on file size, formatting, settings,
software and operating system, such as Microsoft Operating System and/or
pre-installed software applications, or media content. Actual formatted
capacity may vary.
2 A kibibyte (KiB) means 210, or 1,024 bytes, a
mebibyte (MiB) means 220, or 1,048,576 bytes, and a gibibyte
(GiB) means 230, or 1,073,741,824 bytes.
3 MTTF (Mean Time to Failure) is not a guarantee or estimate
of product life; it is a statistical value related to mean failure rates
for a large number of products which may not accurately reflect actual
operation. Actual operating life of the product may be different from
the MTTF.
4 Read and write speed may vary depending on the host device,
read and write conditions, and file size.