The MD06ACA-V Series is Toshiba’s largest capacity surveillance-class HDD
Toshiba
America Electronic Components, Inc., a committed technology leader,
announces the MD06ACA-V, the latest addition to its SV Series line-up of
3.5-inch hard drives for surveillance applications. The new models are
available in capacities up to 10TB1 with a higher transfer
rate compared to previous MD04ABA-V models, helping to enable support
for up to 64 camera2 streams. Higher capacity and transfer
rates enable support for higher resolution camera streams to meet
changing compliance mandates for surveillance data.
The MD06ACA-V Series is designed for 24/7 streaming operation scenarios,
and is typically used for surveillance digital video recorders (SDVR),
surveillance network video recorders (SNVR) and Hybrid SDVR. The
MD06ACA-V Series features 7,200 rpm access performance, and the new 10TB
model delivers a 58 percent increase in maximum sustained transfer rate
when compared to Toshiba’s prior MD04ABA-V series, pushing it to 237MiB/s3.
Available in 6TB, 8TB and 10TB capacities, the new models provide a SATA
6Gbit/s interface4, with a 256MiB dynamic buffer.
Additionally, the MD06ACA-V models support Advanced Format (512e)
technology for compatibility with legacy applications and operating
environments.
“Our third generation surveillance HDD line-up provides the capacity,
performance and reliability needed for today’s higher resolution
surveillance video streams and longer content retention requirements,”
said Scott Wright, Director of HDD Product Marketing at Toshiba America
Electronic Components, Inc. “The new Toshiba models include RV
compensation technology for optimal performance in multi-bay
configurations, and provide excellent reliability with a mean time to
failure (MTTF)5 of 1 million hours utilizing a conventional
mechanical design.”
Samples of the MD06ACA-V Series are now available. For more information
on the full line of Toshiba HDD products, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html.
To learn more about Toshiba storage solutions visit the storage blog at http://storage.toshiba.com/corporateblog/ and
follow @ToshibaStorage
on Twitter.
About Toshiba Group and Toshiba America Electronic Components, Inc.
Through proven commitment, lasting relationships and advanced, reliable
electronic components, Toshiba Group enables its customers to create
market-leading designs. Toshiba Group is the heartbeat within product
breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip
companies worldwide. A committed electronic components leader, Toshiba
Group designs and manufactures high-quality hard disk drives (HDDs),
discrete devices, custom SoCs/ASICs, imaging products, microcontrollers,
wireless components, mobile peripheral devices, and advanced materials
that make possible today’s leading smartphones, tablets, cameras,
medical devices, automotive electronics, industrial applications,
enterprise solutions, consumer products and more.
Toshiba
America Electronic Components, Inc. is an independent operating
company owned by Toshiba America, Inc. For over 140 years, Toshiba
Corporation and its affiliates/subsidiaries have contributed to a
sustainable future by applying innovative technologies to value
creation. Today, our business domains are centered on the essential
infrastructure that supports modern life and society. Guided by the
principles of The Basic Commitment of the Toshiba Group, “Committed to
People, Committed to the Future”, Toshiba Group promotes global
operations that contribute to realization of a world where generations
to come can live better lives. Visit our web site at http://toshiba.semicon-storage.com.
© 2017 Toshiba America Electronic Components, Inc. All rights reserved.
Information in this press release, including product pricing and
specifications, content of services and contact information, is current
and believed to be accurate on the date of the announcement, but is
subject to change without prior notice. Company names, product names,
and service names mentioned herein may be trademarks of their respective
companies.
1 We define a megabyte (MB) as 1,000,000 bytes, a gigabyte
(GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000
bytes. A computer operating system, however, reports storage capacity
using powers of 2 for the definition of 1TB = 240 =
1,099,511,627,776 bytes and therefore shows less storage capacity.
Available storage capacity (including examples of various media files)
will vary based on file size, formatting, settings, software and
operating system and/or pre-installed software applications, or media
content. Actual formatted capacity may vary.
2 Number of surveillance cameras support capability is
defined by performance simulation with High Definition cameras at
10Mbit/s rate. Actual results may vary based on various factors,
including the types of cameras installed, the system’s hardware and
software capabilities, and the video compression technology used, as
well as system variables such as resolution, frames per second, and
other settings.
3 A mebibyte (MiB) means 220, or 1,048,576 bytes.
4 Read and write speed may vary depending on the host device,
read and write conditions, and file size.
5 MTTF (Mean Time to Failure) is not a guarantee or estimate
of product life; it is a statistical value related to mean failure rates
for a large number of products which may not accurately reflect actual
operation. Actual operating life of the product may be different from
the MTTF.