View all news

Toshiba Develops Industry’s First 2200V Dual Silicon Carbide(SiC) MOSFET Module That Contributes to High Efficiency and Downsizing of Industrial Equipment

08/28/2023

Toshiba Electronic Devices & Storage Corporation ("Toshiba") has developed “MG250YD2YMS3,” the industry’s first[1] 2200V dual silicon carbide (SiC) MOSFET module for industrial equipment. The new module has a drain current (DC) rating of 250A and uses the company’s third generation SiC MOSFET chips. It is suitable for applications that use DC1500V, such as photovoltaic power systems and energy storage systems. Volume shipments start today.

Toshiba: MG250YD2YMS3, the industry's first 2200V dual silicon carbide(SiC) MOSFET module. (Graphic: Business Wire)

Toshiba: MG250YD2YMS3, the industry's first 2200V dual silicon carbide(SiC) MOSFET module. (Graphic: Business Wire)

Industrial applications like those mentioned above generally use DC1000V or lower power, and their power devices are mostly 1200V or 1700V products. However, anticipating widespread use of DC1500V in coming years, Toshiba has released the industry’s first 2200V product.

MG250YD2YMS3 offers low conduction loss with a low drain-source on-voltage (sense) of 0.7V (typ.)[2]. It also offers lower turn-on and turn-off switching loss of 14mJ (typ.)[3] and 11mJ (typ.)[3] respectively, an approximately 90% reduction[4] against a typical silicon (Si) IGBT. These characteristics contribute to higher equipment efficiency. Realizing low switching loss also allows the conventional three-level circuit to be replaced with a two-level circuit with a lower module count, contributing to equipment miniaturization.

Toshiba will continue to meet the market needs for high efficiency and the downsizing of industrial equipment.

Notes:
[1] Among dual SiC MOSFET modules. Toshiba survey, as of August 2023.
[2] Test condition: ID=250A, VGS=+20V, Tch=25°C
[3] Test condition: VDD=1100V, ID=250A, Tch=150°C
[4] Toshiba comparison of switching loss for a 2300V Si module and MG250YD2YMS3, the new all SiC MOSFET module, as of August 2023 (performance values for the 2300V Si module is a Toshiba estimate based on papers published in or before March 2023.)

Applications
Industrial Equipment
- Renewable energy power generation systems (photovoltaic power systems, etc.)
- Energy storage systems
- Motor control equipment for industrial equipment
- High frequency DC-DC converter, etc.

Features

  • Low drain-source on-voltage (sense):
    VDS(on)sense=0.7V (typ.) (ID=250A, VGS=+20V, Tch=25°C)
  • Low turn-on switching loss:
    Eon=14mJ (typ.) (VDD=1100V, ID=250A, Tch=150°C)
  • Low turn-off switching loss:
    Eoff=11mJ (typ.) (VDD=1100V, ID=250A, Tch=150°C)
  • Low stray inductance:
    LsPN=12nH (typ.)

Main Specifications

(Tc=25°C unless otherwise specified)

Part number

MG250YD2YMS3

Toshiba’s package name

2-153A1A

Absolute

maximum

ratings

Drain-source voltage VDSS (V)

2200

Gate-source voltage VGSS (V)

+25 / -10

Drain current (DC) ID (A)

250

Drain current (pulsed) IDP (A)

500

Channel temperature Tch (°C)

150

Isolation voltage Visol (Vrms)

4000

Electrical

characteristics

Drain-source on-voltage (sense)

VDS(on)sense (V)

ID=250A, VGS=+20V,

Tch=25°C

typ.

0.7

Source-drain on-voltage (sense)

VSD(on)sense (V)

IS=250A, VGS=+20V,

Tch=25°C

typ.

0.7

Source-drain off-voltage (sense)

VSD(off)sense (V)

IS=250A, VGS=-6V,

Tch=25°C

typ.

1.6

Turn-on switching loss

Eon (mJ)

VDD=1100V,

ID=250A, Tch=150°C

typ.

14

Turn-off switching loss

Eoff (mJ)

typ.

11

Stray inductance LsPN (nH)

typ.

12

Follow the link below for more on the new product.
MG250YD2YMS3

Follow the link below for more on Toshiba’s SiC Power Devices.
SiC Power Devices

* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

About Toshiba Electronic Devices & Storage Corporation
Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.
The company's 21,500 employees around the world share a determination to maximize product value, and promote close collaboration with customers in the co-creation of value and new markets. With annual sales approaching 800-billion yen (US$6.1 billion), Toshiba Electronic Devices & Storage Corporation looks forward to building and to contributing to a better future for people everywhere.
Find out more at https://toshiba.semicon-storage.com/ap-en/top.html

Customer Inquiries:
Power Device Sales & Marketing Dept.
Tel: +81-44-548-2216
Contact Us

Media Inquiries:
Chiaki Nagasawa
Digital Marketing Dept.
Toshiba Electronic Devices & Storage Corporation
semicon-NR-mailbox@ml.toshiba.co.jp

Source: Toshiba Electronic Devices & Storage Corporation

Multimedia Files:

View all news