View all news

Toshiba Launches Small and Thin Common-Drain MOSFET Featuring Very Low On-Resistance Suitable for Quick Charging Devices

05/17/2023

Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched “SSM14N956L,” a 12V common-drain N-channel MOSFET with a current rating of 20A, for use in battery protection circuits in lithium-ion (Li-ion) battery packs, such as those for mobile devices. Shipments start today.

Toshiba: SSM14N956L, a small and thin common-drain MOSFET featuring very low On-resistance (Graphic: Business Wire)

Toshiba: SSM14N956L, a small and thin common-drain MOSFET featuring very low On-resistance (Graphic: Business Wire)

Li-ion battery packs rely on highly robust protection circuits to reduce heat generation while charging and discharging and to enhance safety. These circuits must feature low power consumption and high-density packaging, requiring MOSFETs that are small and thin and that deliver low On-resistance.

SSM14N956L uses Toshiba’s micro-process, as does the already released SSM10N954L. This ensures both low power loss, due to industry-leading[1] low On-resistance characteristics, and low standby power, realized by industry-leading[1] low gate-source leakage current characteristics. These qualities help to extend battery operating hours. The new product also uses a new small, thin package, TCSPED-302701 (2.74mm x 3.0mm, t = 0.085mm (typ.)).

Toshiba will continue to develop MOSFET products for protection circuits in devices powered by lithium-ion battery packs.

Applications

  • Consumer electronics and office and personal devices with a lithium-ion battery pack, including smartphones, tablets, power banks, wearable devices, game consoles, electric toothbrushes, compact digital cameras, digital SLR cameras, etc.

Features

  • Industry leading[1] low On-resistance: RSS(ON)=1.1mΩ (typ.) @VGS=3.8V
  • Industry leading[1] low gate-source leakage current: IGSS=±1μA (max) @VGS=±8V
  • Small and thin type TCSPED-302701 package: 2.74mm x 3.0mm, t=0.085mm (typ.)
  • Common-drain structure that can be easily used in battery protection circuits

Note:
[1]: Among products with the same ratings. As of May 2023, Toshiba survey.

Main Specifications

(Unless otherwise specified, Ta=25°C)

Part number

SSM14N956L

SSM10N954L [2]

Configuration

N-channel common-drain

Absolute
maximum
ratings

Source-source voltage VSSS (V)

12

Gate-source voltage VGSS (V)

±8

Source current (DC) IS (A)

20.0

13.5

Electrical
Characteristics

Gate-source leakage current IGSS

max (μA)

@VGS= ±8V

±1

Source-source
On-resistance RSS(ON)

typ. (mΩ)

@VGS=4.5V

1.00

2.1

@VGS=3.8V

1.10

2.2

@VGS=3.1V

1.25

2.4

@VGS=2.5V

1.60

3.1

Packages

Name

TCSPED-302701

TCSPAC-153001

Size typ. (mm)

2.74x3,

t=0.085

1.49x2.98,

t=0.11

Sample Check & Availability

Buy Online

Buy Online

Note:
[2] Already released product.

Follow the link below for more on the new product.
SSM14N956L

To check availability of the new product at online distributors, visit:
SSM14N956L
Buy Online

* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

About Toshiba Electronic Devices & Storage Corporation

Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.
The company's 21,500 employees around the world share a determination to maximize product value, and promote close collaboration with customers in the co-creation of value and new markets. With annual sales approaching 800-billion yen (US$6.1 billion), Toshiba Electronic Devices & Storage Corporation looks forward to building and to contributing to a better future for people everywhere.
Find out more at https://toshiba.semicon-storage.com/ap-en/top.html

Customer Inquiries
Small Signal Device Sales & Marketing Dept.
Tel: +81-44-548-2215
Contact Us

Media Inquiries:
Chiaki Nagasawa
Digital Marketing Department
Toshiba Electronic Devices & Storage Corporation
semicon-NR-mailbox@ml.toshiba.co.jp

Source: Toshiba Electronic Devices & Storage Corporation

Multimedia Files:

View all news