KAWASAKI, Japan--(BUSINESS WIRE)--
Toshiba Electronic Devices & Storage Corporation ("Toshiba") will this month start to provide test samples of “TB9032FNG,” an automotive driver/receiver IC for the physical layer interface defined in the Clock Extension Peripheral Interface (CXPI) [1] , the standard for automotive communications protocols.
Toshiba: TB9032FNG, an automotive driver/receiver IC for Clock Extension Peripheral Interface(CXPI) (Graphic: Business Wire)
The electrification of automobiles is increasing the number of electronic components in automotive systems, adding to their complexity, and also to vehicle weight, as more wiring harnesses are required. The solution to this issue lies in changing the current system, where a human machine interface (HMI) [2] connects switches and sensors in a one-to-one manner, for a system that uses multiplex transmission in-vehicle communications to reduce wiring harnesses.
HMI integrates an area network (CAN) [3] and a local interconnect network (LIN) [4]; the former is costly, the latter lacks responsiveness. CXPI, the in-vehicle communications protocols developed in Japan, and now adopted as an international standard, includes in-vehicle subnetworks that cost less than CAN and that are more responsive than LIN.
TB9032FNG combines Motor Driver IC and CXPI communications, and provides as a network interface for in-vehicle body applications, or as an interface for zone electronic control units (ECUs) [5]. It can control functions such as door locking and side mirror control.
The new product can be switched between commander node and responder node via an external terminal. In addition, it features current consumption (Sleep) (IBAT_SLP) of 5μA (typ.)[6], with low current consumption on standby. It is also equipped with fault detection functions that include overheat detection and low voltage detection, and is house in a P-SOP8-0405-1.27-002 package.
With an operating temperature range of -40 to 125°C, the product has been designed to conform to AEC-Q100 (Grade1), a qualification standard for automotive electronic components.
Toshiba plans to use the CXPI physical layer technical assets it has cultivated to develop an interface IC that also integrates the CXPI controller and the protocol-control hardware.
Notes:
[1] CXPI (Clock Extension Peripheral Interface): A communications standard, developed in Japan, for in-vehicle sub-networks derived from LIN.
[2] HMI (Human Machine Interface): A mechanism enabling interactions between humans and machines
[3] CAN (Controller Area Network): A serial communications standard, primarily used for automotive communications networks
[4] LIN (Local Interconnect Network): A communications standard for lower-cost, lower-speed on-board subnetworks than provided by CAN
[5] ECU (Electronic Control Unit): Electronic control units, which are primarily installed in motor vehicles
[6] Measuring conditions: VVIO=4.5 to 5.5V, VBAT=7 to 18V, Ta=- 40 to 125°C, NSLP=L, TXD=H, BUS=VBAT
Applications
Automotive equipment
-
Body control system applications (steering wheel switches, meter cluster switches, light switches, door locks, door mirrors, etc.)
-
Zone ECUs
Features
-
Physical layer interface conforming to CXPI, the standard for automotive communications protocols
-
High-speed response suitable for automotive body system applications (compared with LIN[3])
-
Switchable between commander node and responder node via an external terminal
-
Built-in sleep mode
-
Low current consumption (Sleep) : IBAT_SLP=5μA (typ.)
-
Various fault detection functions: overheat detection, low voltage detection and dominant timeout
-
P-SOP8-0405-1.27-002 package
-
To be AEC-Q100 (Grade1) qualified
Main Specifications
|
|
(Ta=-40 to 125°C unless otherwise specified)
|
|
Part number
|
TB9032FNG
|
|
Standard
|
ISO 20794-4 (Automotive communications protocol standard CXPI physical layer)
|
|
Function
|
Physical layer interface
|
|
Nodes selection
|
Possible
(Switchable between the commander node and responder node via an external terminal.)
|
|
Absolute maximum ratings
|
Power supply voltage 1 VBAT (V)
|
Ta=25°C
|
-0.3 to 40
|
|
Operating ranges
|
BAT normal operating range VBAT (V)
|
7 to 18
|
|
VIO normal operating range VVIO (V)
|
4.5 to 5.5
|
|
Operating temperature range Ta (°C)
|
-40 to 125
|
|
Current consumption (Sleep) IBAT_SLP (μA)
|
typ.
|
5
|
|
Communications speed (kbps)
|
max
|
20
|
|
Fault detection functions
|
Overheat detection, low voltage detection and dominant timeout
|
|
Package
|
Name
|
P-SOP8-0405-1.27-002
|
|
Size (mm)
|
typ.
|
6.0×4.9
|
|
Reliability test
|
To be AEC-Q100 (Grade1) qualified
|
|
Mass production
|
March 2024
|
|
|
|
|
|
Follow the links below for more on the new product.
TB9032FNG
Follow the link below for more on Toshiba’s products for automotive network communications.
Automotive Network Communications
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.
About Toshiba Electronic Devices & Storage Corporation
Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.
The company's 23,000 employees around the world share a determination to maximize product value, and promote close collaboration with customers in the co-creation of value and new markets. With annual sales now surpassing 850-billion yen (US$7.5 billion), Toshiba Electronic Devices & Storage Corporation looks forward to building and to contributing to a better future for people everywhere.
Find out more at https://toshiba.semicon-storage.com/ap-en/top.html
Source: Toshiba Electronic Devices & Storage Corporation