View all news

Toshiba Launches 2:1 Multiplexer/1:2 Demultiplexer Switches that Support High-Speed Differential Signal Such as PCIe® 5.0 and USB4®

07/10/2024

Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has launched “TDS4A212MX” and “TDS4B212MX,” multiplexer/demultiplexer (Mux/De-Mux) switches for high-speed differential signals such as PCIe® 5.0, USB4® and USB4® Ver.2, for PCs, server equipment, mobile devices and more. The new products can be used as a 2-input 1-output Mux switch and a 1-input 2-output De-Mux switch. Shipments start today.

Toshiba: "TDS4A212MX" and "TDS4B212MX," multiplexer/demultiplexer switches for high-speed differential signals such as PCIe® 5.0, USB4® and USB4® Ver.2, for PCs, server equipment and more. (Graphic: Business Wire)

Toshiba: "TDS4A212MX" and "TDS4B212MX," multiplexer/demultiplexer switches for high-speed differential signals such as PCIe® 5.0, USB4® and USB4® Ver.2, for PCs, server equipment and more. (Graphic: Business Wire)

The new products use Toshiba's proprietary SOI process (TarfSOI™) to achieve very high bandwidths: an industry-leading[1] -3-dB bandwidth (differential) of 27.5GHz(typ.) for TDS4B212MX, and 26.2GHz(typ.) for TDS4A212MX. This allows the new products to be used as a Mux/De-Mux switch for high-speed differential signals such as PCIe® 5.0, USB4® and USB4® Ver.2.

TDS4B212MX and TDS4A212MX have different pin assignments. That of TDS4B212MX is optimized for high-frequency characteristics. TDS4A212MX has a pin assignment that considers circuit board layout.

Note:

[1] As a 2:1 Mux/1:2 De-Mux switch, as of July 11, 2024, Toshiba survey.

Applications

  • PCs, server equipment, mobile devices, wearable devices, etc.

    Supported interfaces: PCIe® 5.0, PCIe® 4.0, PCIe® 3.0, CXL2.0, CXL1.0, USB4® Ver.2, USB4®, USB3.2 Gen2×1, USB3.2 Gen1×1, Thunderbolt™ 4, Thunderbolt™ 3, Thunderbolt™ 2, DisplayPort™ 2.0, DisplayPort™ 1.4, DisplayPort™ 1.3, DisplayPort™ 1.2

Features

  • High -3-dB bandwidth (differential) for high-speed differential signal such as PCIe® 5.0 and USB4®

    TDS4B212MX: -3-dB bandwidth (differential)=27.5GHz (typ.)

    TDS4A212MX: -3-dB bandwidth (differential)=26.2GHz (typ.)
  • Low current consumption: Iope=150μA (max)
  • Small package: XQFN16 (2.4mm×1.6mm (typ.), t=0.4mm (max))

Main Specifications

Part number

TDS4B212MX

TDS4A212MX

Package

Name

XQFN16

Size (mm)

2.4×1.6 (typ.), t=0.4 (max)

Operating ranges

(Ta=-40 to 85°C)

Supply voltage VCC (V)

1.6 to 3.6

Signal pins differential voltage (peak to peak) VI/O(Diff) (V)

0 to 1.8

Signal pins common mode voltage VI/O(Com) (V)

0 to 2.0

DC characteristics

(Ta=-40 to 85°C)

Standby current ISTB (μA)

Max

10

Current consumption Iope (μA)

Max

150

High frequency

characteristics

(Ta=25°C)

-3-dB bandwidth (differential)

BW(Diff) (GHz)

Typ.

27.5

26.2

Differential insertion loss

DDIL (dB)

f=5.0GHz

Typ.

-0.8

-0.9

f=8.0GHz

-0.9

-1.0

f=10.0GHz

-0.9

-1.1

f=12.8GHz

-1.2

-1.4

f=16.0GHz

-1.4

-1.9

Differential return loss

DDRL (dB)

f=5.0GHz

Typ.

-17

-15

f=8.0GHz

-15

-14

f=10.0GHz

-20

-17

f=12.8GHz

-17

-17

f=16.0GHz

-16

-18

Differential OFF isolation

DDOIRR (dB)

f=5.0GHz

Typ.

-20

-20

f=8.0GHz

-17

-19

f=10.0GHz

-16

-17

f=12.8GHz

-17

-12

f=16.0GHz

-14

-11

Differential crosstalk

DDXT (dB)

f=5.0GHz

Typ.

-56

-36

f=8.0GHz

-48

-34

f=10.0GHz

-44

-32

f=12.8GHz

-39

-31

f=16.0GHz

-36

-30

Sample Check & Availability

Buy Online

Buy Online

Follow the links below for more on the new products.

TDS4A212MX

TDS4B212MX

Follow the link below for more on Toshiba’s General Purpose Logic ICs.

General Purpose Logic ICs

To check availability of the new products at online distributors, visit:

TDS4A212MX

Buy Online

TDS4B212MX

Buy Online

*USB4® is a registered trademark of USB Implementers Forum.

*Thunderbolt™ is a trademark of Intel Corporation or its subsidiaries.

*DisplayPort™ is a trademark or registered trademark of the Video Electronics Standards Association in the United States and other countries.

*PCIe® is a registered trademark of PCI-SIG.

*TarfSOI™ is a trademark of Toshiba Electronic Devices & Storage Corporation.

*Other company names, product names, and service names may be trademarks of their respective companies.

* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

About Toshiba Electronic Devices & Storage Corporation

Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.

Its 19,400 employees around the world share a determination to maximize product value, and to promote close collaboration with customers in the co-creation of value and new markets. The company looks forward to building and to contributing to a better future for people everywhere.

Find out more about TDSC at https://toshiba.semicon-storage.com/ap-en/top.html

Customer Inquiries:

Power & Small Signal Device Sales & Marketing Dept.II

Tel: +81-44-548-2215

Contact Us

Media Inquiries:

Chiaki Nagasawa

Digital Marketing Dept.

Toshiba Electronic Devices & Storage Corporation

semicon-NR-mailbox@ml.toshiba.co.jp

Source: Toshiba Electronic Devices & Storage Corporation

Multimedia Files:

Toshiba: "TDS4A212MX" and "TDS4B212MX," multiplexer/demultiplexer switches for high-speed differential signals such as PCIe® 5.0, USB4® and USB4® Ver.2, for PCs, server equipment and more. (Graphic: Business Wire) 1200 x 628 jpg 339 KB
View all news