- Four new devices boost efficiency and power density of industrial equipment -
KAWASAKI, Japan--(BUSINESS WIRE)--
Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched four 650V silicon carbide (SiC) MOSFETs, equipped with its latest[1] 3rd generation SiC MOSFET chips and housed in a compact DFN8x8 package, suitable for industrial equipment, such as switched-mode power supplies and power conditioners for photovoltaic generators. Volume shipments of the four devices, “TW031V65C,” “TW054V65C,” “TW092V65C,” and “TW123V65C,” start today.

Toshiba: 650V 3rd generation SiC MOSFETs in DFN8x8 package
The new products are the first 3rd generation SiC MOSFETs to use the small surface-mount DFN8x8 package, which reduces volume by more than 90% compared to lead-inserted packages, such as TO-247 and TO-247-4L(X) and improves equipment power density. Surface mounting also allows use of parasitic impedance[2] components smaller than those of lead-inserted packages, reducing switching losses. DFN8x8 is a 4-pin[3] package, allowing use of a Kelvin connection of its signal source terminal for the gate drive. This reduces the influence of inductance in the source wire within the package, achieving high-speed switching performance; in the case of TW054V65C, it reduces turn-on loss by approximately 55% and turn-off loss by approximately 25%[4] compared to current Toshiba products[5], helping to reduce power loss in equipment.
Toshiba will continue to expand its lineup to contribute to improved equipment efficiency and increased power capacity.
Notes:
[1] As of May 2025.
[2] Resistance, inductance, etc.
[3] A product with a signal-source pin connected close to the FET chip.
[4] As of May 2025, values measured by Toshiba. For details, see Figure 1 in the version of this release on the Toshiba website.
[5] A 650V 3rd generation SiC MOSFET with equivalent voltage and On-resistance that uses the TO-247 package without Kelvin connection.
Applications
- Switched mode power supplies in servers, data centers, communications equipment, etc.
- EV charging stations
- Photovoltaic inverters
- Uninterruptible power supplies
Features
- DFN8x8 surface-mount package. Enables equipment miniaturization of and automated assembly. Low switching loss.
- Toshiba’s 3rd generation SiC MOSFETs
- Good temperature dependence of drain-source On-resistance by optimization of drift resistance and channel resistance ratio
- Low drain-source On-resistance x gate-drain charges
- Low diode forward voltage: VDSF =-1.35V(typ.) (VGS =-5V)
Main Specifications
| (Unless otherwise specified, Ta=25℃) |
Part number | TW031V65C | TW054V65C | TW092V65C | TW123V65C |
Package | Name | DFN8x8 |
Size (mm) | Typ. | 8.0×8.0×0.85 |
Absolute maximum ratings | Drain-source voltage VDSS (V) | 650 |
Gate-source voltage VGSS (V) | -10 to 25 |
Drain current (DC) ID (A) | Tc=25°C | 53 | 36 | 27 | 18 |
Electrical characteristics | Drain-Source On-resistance RDS(ON) (mΩ) | VGS=18V | Typ. | 31 | 54 | 92 | 123 |
Gate threshold voltage Vth (V) | VDS=10V | 3.0 to 5.0 |
Total gate charge Qg (nC) | VGS=18V | Typ. | 65 | 41 | 28 | 21 |
Gate-drain charge Qgd (nC) | VGS=18V | Typ. | 10 | 6.2 | 3.9 | 2.3 |
Input capacitance Ciss (pF) | VDS=400V | Typ. | 2288 | 1362 | 873 | 600 |
Diode forward voltage VDSF (V) | VGS=-5V | Typ. | -1.35 |
Sample Check & Availability | Buy Online | Buy Online | Buy Online | Buy Online |
Related links
Features of third generation SiC MOSFET
FAQ SiC MOSFET
Comparison of SiC MOSFET and Si IGBT
SiC MOSFET Absolute Maximum Ratings and Electrical Characteristics
Follow the links below for more on the new products.
TW031V65C
TW054V65C
TW092V65C
TW123V65C
Follow the link below for more on Toshiba’s SiC Power Devices.
SiC Power Devices
To check availability of the new products at online distributors, visit:
TW031V65C
Buy Online
TW054V65C
Buy Online
TW092V65C
Buy Online
TW123V65C
Buy Online
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.
About Toshiba Electronic Devices & Storage Corporation
Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.
Its 19,400 employees around the world share a determination to maximize product value, and to promote close collaboration with customers in the co-creation of value and new markets. The company looks forward to building and to contributing to a better future for people everywhere.
Find out more at https://toshiba.semicon-storage.com/ap-en/top.html
Source: Toshiba Electronic Devices & Storage Corporation