- Three new devices boost efficiency and power density of industrial equipment -
KAWASAKI, Japan--(BUSINESS WIRE)--
Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched three 650V silicon carbide (SiC) MOSFETs equipped with its latest[1] 3rd generation SiC MOSFET chips and housed in surface-mount TOLL packages. The new devices are suitable for industrial equipment, such as switched-mode power supplies and power conditioners for photovoltaic generators. Volume shipments of the MOSFETs, “TW027U65C,” “TW048U65C,” and “TW083U65C,” start today.

Toshiba: 650V 3rd generation SiC MOSFETs in TOLL package.
The new products are Toshiba’s 3rd generation SiC MOSFETs in a general-purpose surface-mount TOLL package, which reduces device volume by more than 80% compared to through-hole packages such as TO-247 and TO-247-4L(X), and improves equipment power density.
The TOLL package also offers lower parasitic impedance[2] than through-hole packages, which helps to reduce switching losses. As a 4-terminal[3] package, a Kelvin connection can be used as the signal source terminal for the gate drive. This reduces the influence of inductance in the source wire within the package, achieving high-speed switching performance; in the case of TW048U65C, turn-on loss and turn-off loss are approximately 55% and 25%[4] lower, respectively, than in current Toshiba products[5], which will contribute to lower equipment power loss.
Toshiba will continue to expand its lineup to contribute to improved equipment efficiency and increased power capacity.
Notes:
[1] As of August 2025.
[2] Resistance, inductance, etc.
[3] A product with a signal-source terminal connected close to the FET chip.
[4] As of August 2025, values measured by Toshiba. For details, see Figure 1 in the version of this release on the Toshiba website.
[5] A 650V 3rd generation SiC MOSFET with equivalent voltage and On-resistance that uses the TO-247 package without Kelvin connection.
Applications
- Switched-mode power supplies in servers, data centers, communications equipment, etc.
- EV charging stations
- Photovoltaic inverters
- Uninterruptible power supplies
Features
- Surface-mount TOLL package: Enables equipment miniaturization and automated assembly. Low switching loss.
- Toshiba’s 3rd generation SiC MOSFETs:
- Optimization of drift resistance and channel resistance ratio realizes good temperature dependence of drain-source On-resistance.
- Low drain-source On-resistance×gate-drain charges
- Low diode forward voltage: V DSF =-1.35V(typ.) (V GS =-5V)
| Main Specifications |
(Unless otherwise specified, Ta=25℃) |
Part number | TW027U65C | TW048U65C | TW083U65C |
Package | Name | TOLL |
Size (mm) | Typ. | 9.9×11.68×2.3 |
Absolute
maximum
ratings | Drain-source voltage VDSS (V) | 650 |
Gate-source voltage VGSS (V) | -10 to 25 |
Drain current (DC) ID (A) | Tc=25°C | 57 | 39 | 28 |
Electrical
characteristics | Drain-Source On-resistance RDS(ON) (mΩ) | VGS=18V | Typ. | 27 | 48 | 83 |
Gate threshold voltage Vth (V) | VDS=10V | 3.0 to 5.0 |
Total gate charge Qg (nC) | VGS=18V | Typ. | 65 | 41 | 28 |
Gate-drain charge Qgd (nC) | VGS=18V | Typ. | 10 | 6.2 | 3.9 |
Input capacitance Ciss (pF) | VDS=400V | Typ. | 2288 | 1362 | 873 |
Diode forward voltage VDSF (V) | VGS=-5V | Typ. | -1.35 |
Sample Check & Availability | Buy Online | Buy Online | Buy Online |
Follow the links below for more on the new product.
TW027U65C
TW048U65C
TW083U65C
Follow the link below for more on Toshiba’s SiC Power Devices.
SiC Power Devices
To check availability of the new products at online distributors, visit:
TW027U65C
Buy Online
TW048U65C
Buy Online
TW083U65C
Buy Online
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.
About Toshiba Electronic Devices & Storage Corporation
Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.
Its 19,400 employees around the world share a determination to maximize product value, and to promote close collaboration with customers in the co-creation of value and new markets. The company looks forward to building and to contributing to a better future for people everywhere.
Find out more at https://toshiba.semicon-storage.com/ap-en/top.html
Source: Toshiba Electronic Devices & Storage Corporation