KAWASAKI, Japan--(BUSINESS WIRE)--
Toshiba Electronic Devices & Storage Corporation
("Toshiba") has launched "
TLP3414S
” and “
TLP3431S," photorelays housed in the S-VSON4T[1]
package that feature a faster turn-on time than Toshiba’s current products[2]
. The OFF-state output terminal voltage rating and the ON-state current rating of TLP3414S are 40V/250mA and those of TLP3431S are 20V/450mA. Shipments start today.

Toshiba: small photorelays TLP3414S and TLP3431S that help shorten test time for semiconductor testers (Graphic: Business Wire)
The new photorelays achieve high efficiency optical coupling with improved optical output from the input side infrared-emitting diodes and optimization of photo detectors (photodiode arrays). This realizes a high speed turn-on time, a maximum of 150μs. The turn-on time of TLP3414S is approximately 50% shorter than that of Toshiba’s current product, TLP3414, and that of the TLP3431S is approximately 62% shorter than Toshiba’s current TLP3431.
In addition, ON-state resistance, which affects signal attenuation when the output is turned on (TLP3414S: maximum 3Ω, TLP3431S: maximum 1.2Ω), and output capacitance, which affects high frequency signal leakage when the output is turned off (both TLP3414S and TLP3431S: typical 6.5pF), are equivalent to those of existing Toshiba products[2]
, and deliver stable signal transmission.
The new products are suitable for pin electronics[3]
applications in semiconductor testers, which measure devices under test (DUT) with high accuracy and at high speed while switching signals.
The package uses the small S-VSON4T package, reducing the mounting area by approximately 20% compared to the VSON4 package[4]
of Toshiba’s current product. This contributes to the miniaturization of semiconductor testers and others.
Toshiba will continue to provide products that meet the demands for higher performance and faster speeds in semiconductor testers.
Notes: |
[1] S-VSON4T package : 1.45×2.0mm (typ.) |
[2] Toshiba’s existing products TLP3414 (ratings 40V/250mA) and TLP3431 (ratings 20V/450mA) in a VSON4 package. |
[3] Pin electronics (PE): An interface circuit for supplying power and test signals to the DUT, and for judging output signals from the DUT. |
[4] VSON4 package: 1.45×2.45mm (typ.) |
Applications
- Semiconductor testers (high speed memory testers, high speed logic testers, etc.)
- Probe cards
- Measurement equipment
Features
- High speed turn-on time: tON=150μs (max)
- Low ON-state resistance
TLP3414S RON=3Ω (max)
TLP3431S RON=1.2Ω (max) - Small S-VSON4T package: 1.45×2.0mm (typ.), t=1.3mm (typ.)
Main Specifications
(T
a
=25°C) |
Part number | TLP3414S | TLP3431S |
Package | Toshiba’s name | S-VSON4T |
Size (mm) | 1.45×2.0 (typ.), t=1.3 (typ.) |
Contact type | 1-Form-A (Normally opened) |
Absolute maximum ratings | OFF-state output terminal voltage V
OFF
(V) | 40 | 20 |
ON-state current I
ON
(mA) | 250 | 450 |
ON-state current (pulsed) I
ONP
(mA) | 750 | 1350 |
Operating temperature T
opr
(°C) | -40 to 110 |
Isolation voltage BV
S
(Vrms) | AC, 60s, R.H.≤60% | 500 |
Coupled electrical characteristics | Trigger LED current I
FT
(mA) | Max | 3 |
ON-state resistance R
ON
(Ω) | Typ. | 2 | 0.8 |
Max | 3 | 1.2 |
Electrical characteristics | Output capacitance C
OFF
(pF) | Typ. | 6.5 |
Switching characteristics | Turn-on time t
ON
(μs) | Max | 150[5] |
Turn-off time t
OFF
(μs) | 100[5] |
Sample Check & Availability | Buy Online | Buy Online |
Note |
[5] Test condition of TLP3414S: R
L
=200Ω, V
DD
=20V, I
F
=5mA, TLP3431S: R
L
=200Ω, V
DD
=10V, I
F
=5mA |
Related information
Technical Articles
Small photorelay with high-speed switching
Compact photorelays with low voltage drive and high temperature operation rating
Follow the links below for more on the new products.
TLP3414S
TLP3431S
Follow the link below for more on Toshiba’s isolators and solid state relays.
Isolators/Solid State Relays
To check availability of the new products at online distributors, visit:
TLP3414S
Buy Online
TLP3431S
Buy Online
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.
About Toshiba Electronic Devices & Storage Corporation
Toshiba Electronic Devices & Storage Corporation, a leading supplier of advanced semiconductor and storage solutions, draws on over half a century of experience and innovation to offer customers and business partners outstanding discrete semiconductors, system LSIs and HDD products.
Its 19,400 employees around the world share a determination to maximize product value, and to promote close collaboration with customers in the co-creation of value and new markets. The company looks forward to building and to contributing to a better future for people everywhere.
Find out more at
https://toshiba.semicon-storage.com/ap-en/top.html
Source: Toshiba Electronic Devices & Storage Corporation